The roentgen or röntgen () (symbol R) is a legacy unit of measurement for the exposure of X-rays and gamma rays, and is defined as the electric charge freed by such radiation in a specified volume of air divided by the mass of that air.
In 1928 it was adopted as the first international measurement quantity for ionising radiation to be defined for radiation protection, as it was then the most easily replicated method of measuring air ionization by using ion chambers. It is named after the German physicist Wilhelm Röntgen, who discovered X-rays.
However, although this was a major step forward in standardising radiation measurement, the roentgen has the disadvantage that it is only a measure of air ionisation, and not a direct measure of radiation absorption in other materials, such as different forms of human tissue. As the science of radiation dosimetry developed, it was realised that the ionising effect, and hence tissue damage, was linked to the energy absorbed, not just radiation exposure. Consequently new radiometric units for radiation protection were defined which took this into account. In 1953 the International Commission on Radiation Units and Measurements (ICRU) recommended the rad, equal to 100 erg/g, as the unit of measure of the new radiation quantity absorbed dose. The rad was expressed in coherent cgs units.
In 1975 the unit gray was named as the SI unit of absorbed dose. The gray is equal to 100 rad, the cgs unit. Additionally, a new quantity Kerma was defined for air ionisation as the exposure quantity for instrument calibration, and from this the absorbed dose can be calculated using known coefficients for specific target materials. Today, for radiation protection, the modern units, absorbed dose for energy absorption and the equivalent dose for stochastic effect, are overwhelmingly used, and the roentgen is rarely used. The International Committee for Weights and Measures (CIPM) has never accepted the use of the roentgen.
The roentgen has been metrologically redefined over the years. It was last defined by the US National Institute of Standards and Technology (NIST) in 1998 as 2.58×10−4 C/kg, with a recommendation that the definition be given in every document where the roentgen is used. One roentgen deposits 0.00877 grays (0.877 rads) of absorbed dose in dry air, or 0.0096 Gy (0.96 rad) in soft tissue. One roentgen of X-rays may deposit anywhere from 0.01 to 0.04 Gy (1.0 to 4.0 rad) in bone depending on the beam energy.