The Lister Storm was a homologated racing car built by Lister Cars of the United Kingdom beginning in 1993. The Storm used the largest V12 engine fitted to a production road car since World War II, a 6,996 cc (6.996 L; 426.9 cu in) Jaguar unit based on the one used in the Jaguar XJR Sportscars that competed at the 24 Hours of Le Mans. Due to the high US $350,000 price of the vehicle, only four examples were produced before production of the road-going Storm ceased. Only three Storms survive today, although the Lister company continues to maintain racing models.
The bored and stroked two-valve Lister V12 produced 407 kW (546 hp) and 790 N·m (582.7 lb·ft) of torque. The front-engined rear-wheel drive car weighed 1,664 kg (3,668.5 lb), and was capable of sprinting to 60 mph (97 km/h) in just 4.1 seconds. Until the launch of the Brabus Rocket, in 2006, it was the fastest four-seater saloon in the world.