powered by CADENAS

Social Share

Amazon

Major appliance (6215 views - Electronics & PCB Engineering)

A major appliance, or domestic appliance, is a large machine in home appliance used for routine housekeeping tasks such as cooking, washing laundry, or food preservation. An appliance is different from a plumbing fixture because it uses electricity or fuel. Major appliances differ from small appliances because they are bigger and not portable. They are often considered fixtures and part of real estate and as such they are often supplied to tenants as part of otherwise unfurnished rental properties. Major appliances may have special electrical connections, connections to gas supplies, or special plumbing and ventilation arrangements that may be permanently connected to the appliance. This limits where they can be placed in a home. Many major appliances are made of enamel-coated sheet steel which, in the middle 20th century, was usually white. The term white goods in contrast to brown goods, is also used, primarily where British English is spoken, although definitions for the term "white goods" can differ. Many appliances nowadays would be considered brown goods, some being connected to the Internet. In the United States, the term white goods can also refer to linens. In New Zealand "whiteware" may be used, elsewhere a term from pottery. Since major appliances in a home consume a significant amount of energy, they have become the objectives of programs to improve their energy efficiency in many countries. Energy efficiency improvements may require changes in construction of the appliances, or improved control systems.
Go to Article

Explanation by Hotspot Model

Youtube


    

Major appliance

Major appliance

A major appliance, or domestic appliance, is a large machine in home appliance used for routine housekeeping tasks such as cooking, washing laundry, or food preservation. An appliance is different from a plumbing fixture because it uses electricity or fuel.

Major appliances differ from small appliances because they are bigger and not portable. They are often considered fixtures and part of real estate and as such they are often supplied to tenants as part of otherwise unfurnished rental properties. Major appliances may have special electrical connections, connections to gas supplies, or special plumbing and ventilation arrangements that may be permanently connected to the appliance. This limits where they can be placed in a home.

Many major appliances are made of enamel-coated sheet steel which, in the middle 20th century, was usually white. The term white goods in contrast to brown goods, is also used, primarily where British English is spoken, although definitions for the term "white goods" can differ. Many appliances nowadays would be considered brown goods, some being connected to the Internet. In the United States, the term white goods can also refer to linens.[1] In New Zealand "whiteware" may be used, elsewhere a term from pottery.[2] Since major appliances in a home consume a significant amount of energy, they have become the objectives of programs to improve their energy efficiency in many countries. Energy efficiency improvements may require changes in construction of the appliances, or improved control systems.

Brands

In the early days of electrification, many major consumer appliances were made by the same companies that made the generation and distribution equipment.[citation needed] While some of these brand names persist to the present day, even if only as licensed use of old popular brand names, today many major appliances are manufactured by companies or divisions of companies that specialize particular appliances.

Types

Major appliances may be roughly divided as follows:[3]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB Engineering

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics