powered by CADENAS

Social Share

Amazon

Swage nut (8675 views - Maschinenbau)

A swage nut or self-clinching nut is a type of nut or threaded insert is used on sheet metal. PEM nut is a brand name by Penn Engineering & Manufacturing Corp often used generically for swage nuts from any manufacturer. It permanently anchors itself to the sheet metal by swaging the surrounding material. Generally, the swage nut is made of a hard metal such as stainless steel, which is inserted into a pre-drilled hole in a softer ductile material such as aluminum. The inserted shank has three diameters: a main shaft which fits the hole closely, a thin smaller-diameter undercut, and a larger-diameter serrated clinching ring. Forcing the clinching ring into softer material, with an arbor press or by tightening a screw through the hole, causes it to plastically deform (swage) into the annular recess in the shank. This locks the nut into the hole. The knurling on the clinching ring is not necessary for this step, but prevents the nut from rotating after installation. This is a popular method for adding strong, load-bearing threads to a relatively thin piece of soft sheet metal. Self-clinching nuts are described in military specification MIL-N-45938.
Go to Article

Youtube

How to use blind rivets, commonly known as pop rivets to join two pieces of thin metal together. This video also shows how to remove rivets.

Swage nut

Swage nut

A swage nut or self-clinching nut is a type of nut or threaded insert is used on sheet metal. PEM nut is a brand name by Penn Engineering & Manufacturing Corp often used generically for swage nuts from any manufacturer.

It permanently anchors itself to the sheet metal by swaging the surrounding material. Generally, the swage nut is made of a hard metal such as stainless steel, which is inserted into a pre-drilled hole in a softer ductile material such as aluminum. The inserted shank has three diameters: a main shaft which fits the hole closely, a thin smaller-diameter undercut, and a larger-diameter serrated clinching ring. Forcing the clinching ring into softer material, with an arbor press or by tightening a screw through the hole, causes it to plastically deform (swage) into the annular recess in the shank. This locks the nut into the hole. The knurling on the clinching ring is not necessary for this step, but prevents the nut from rotating after installation.[1]

This is a popular method for adding strong, load-bearing threads to a relatively thin piece of soft sheet metal.

Self-clinching nuts are described in military specification MIL-N-45938.[2]

History

Albert Spokes filed for a U.S. patent on the swage nut in early 1958.[3] The swage nut is descended from an older idea, the clinch nut. Clinch nuts incorporate a tubular shaft that fits through the part to be attached and is clinched or riveted in place from the opposite side.[4][5]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Example Part

Maschinenbau

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD