Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Aircraft canopy" – news · newspapers · books · scholar · JSTOR (July 2017) (Learn how and when to remove this template message) |
An aircraft canopy is the transparent enclosure over the cockpit of some types of aircraft. An aircraft canopy provides a controlled and sometimes pressurized environment for the aircraft's occupants, and allows for a greater field of view over a traditional flight deck. A canopy's shape is a compromise designed to minimize aerodynamic drag, while maximizing visibility for pilots and other crewmembers.
Very early aircraft had no canopies at all. The pilots were exposed to the wind and weather, although most flying was done in good weather. Through World War I most aircraft had no canopy, although they often had a small windshield to deflect the prop wash and wind from hitting the pilot in the face. In the 1920s and 1930s, the increasing speed and altitude of airplanes necessitated a fully enclosed cockpit and canopies became more common.
Early canopies were made of numerous pieces of flat glass held in position by a frame and muntins. The muntins reduced visibility, which was especially problematic for military aircraft. Also, glass canopies were much heavier than acrylic canopies, which were first introduced shortly before World War II. The acrylic bubble canopy was used on aircraft such as the Supermarine Spitfire and Westland Whirlwind, which gave better all-round visibility and reduced weight. It is still being used today on most fighter aircraft.
In the 1970s, US aviation artist Keith Ferris invented a false canopy to paint on the underside of military aircraft, directly underneath the front of the plane, the purpose of which was to confuse an enemy so they do not know in what direction the aircraft is headed. This ruse was inspired by animals and fishes that have similar markings on the head and tail, so they can confuse other creatures. Pilots remain skeptical of this feature, asserting that if the enemy is close enough to see the marking, they are too close to be fooled by it.[citation needed]
On many high-performance military aircraft, the canopy is an integral part of the ejection seat system. The pilot cannot be ejected from the aircraft until the canopy is no longer in the path of the ejection seat. In most ejection seat equipped aircraft, the canopy is blown upwards and rearwards by explosive charges. The relative wind then blows the canopy away from the ejection path. However, on some aircraft, such as the McDonnell Douglas AV-8B Harrier II, the pilot may be forced to eject when in a hover, or when going too slow for the relative wind to move the canopy out of the path of the ejection seat. In that situation, the pilot could possibly impact the canopy when ejecting. To overcome that possibility, some aircraft have a thin cord of plastic explosive zig-zagging across the canopy over the pilot's head. In the event of an ejection, the explosive cord is activated first, shattering the canopy. Then the ejection seat and pilot is launched through the shattered canopy.
Most modern acrylic canopies are vacuum formed. A sheet of acrylic is secured to a female mould, then the entire assembly is heated in an oven until the acrylic is pliable. The air is then removed from the mould and the acrylic sheet is drawn into it, forming the shape of the canopy. The acrylic is then trimmed to the appropriate shape and attached to an aluminum or composite frame. Some one-off canopies are made in a similar fashion, but since a mould would be too time-consuming to make, the acrylic is heated and vacuum formed until it approximates the shape the builder is seeking. This type of construction is less precise, however, and each canopy is unique. If multiple canopies will be needed, a mould is almost always used.
Have Glass is the code name for a series of RCS reduction measures for the F-16 fighter. Its primary aspect is the addition of an indium-tin-oxide layer to the gold tinted cockpit canopy, which is reflective to radar frequencies. An ordinary canopy would let radar signals straight through where they would strike the many edges and corners inside and bounce back strongly to the radar source, the reflective layer dissipates these signals instead. Overall, Have Glass reduces an F-16's RCS (radar-cross section) by some 15 percent. The gold tint also reduces glare from the sun to improve the pilot's visibility.
The Malcolm Hood is a type of aircraft canopy originally developed for the Supermarine Spitfire. Its concept proved valuable for other aircraft such as the North American Aviation-produced P-51B & C Mustangs as retrofit items, and standard on later versions of the Vought F4U Corsair, and somewhat emulated on the later models of the Luftwaffe's Focke-Wulf Fw 190 fighter.
The canopy was manufactured by the British company R Malcolm & Co which gave its name. Instead of taking a straight line between the canopy frames, the hood was bulged outward. This gave the pilot a better view to the rear.
...the Corsair's initial deficiencies were being worked out on a concurrent basis... The 689th production F4U-1 featured a number of significant changes. The most noticeable was that the cockpit was raised 18 centimeters (7.1 inches) to improve the pilot's forward view, and a bulged canopy, along the lines of the "Malcolm Hood" used on Spitfires, replaced the original "birdcage" framed canopy to provide better all-round field of view.[1]
Hawker Hurricane with canopy slid to rear
An A-10 Thunderbolt II with painted "false canopy" underneath the front of the plane
The low drag canopy of an Extra 300 aerobatic light aircraft.
Sukhoi Su-57 prototype at MAKS 2011
Sukhoi Su-35 at MAKS 2011
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht