powered by CADENAS

Social Share

Amazon

Cosworth DFV (11390 views - Cars & Motorbikes & Trucks & Buse)

The DFV is an internal combustion engine that was originally produced by Cosworth for Formula One motor racing. The name is an abbreviation of Double Four Valve, the engine being a V8 development of the earlier four-cylinder FVA, which had four valves per cylinder.Its development in 1967 for Colin Chapman's Team Lotus was sponsored by Ford. For many years it was the dominant engine in Formula One, and it was also used in other categories of racing, including CART, Formula 3000 and sportscar racing. The engine is a 90°, 2,993 cc V8 with a bore and stroke of 85.67 x 64.897 mm (3.373 x 2.555 in) producing over 400 bhp (408 bhp at 9,000 rpm, 270 ft⋅lbf (370 N⋅m) torque at 7,000 rpm was quoted) from the start reaching over 500 bhp (510 bhp at 11,200 rpm was quoted) by the end of its Formula 1 career. The 1983 DFY variant had a revised bore and stroke of 90 x 59 mm (3.543 x 2.316 in) giving 2,993 cc and 520–530 bhp at 11,000 rpm, 280 ft⋅lbf (380 N⋅m) torque at 8,500 rpm.
Go to Article

Explanation by Hotspot Model

Youtube


    

Cosworth DFV

Cosworth DFV

The DFV is an internal combustion engine that was originally produced by Cosworth for Formula One motor racing. The name is an abbreviation of Double Four Valve, the engine being a V8 development of the earlier four-cylinder FVA, which had four valves per cylinder.[1]

Its development in 1967 for Colin Chapman's Team Lotus was sponsored by Ford. For many years it was the dominant engine in Formula One, and it was also used in other categories of racing, including CART, Formula 3000 and sportscar racing.

The engine is a 90°, 2,993 cc V8 with a bore and stroke of 85.67 x 64.897 mm (3.373 x 2.555 in) producing over 400 bhp (408 bhp at 9,000 rpm, 270 ft⋅lbf (370 N⋅m) torque at 7,000 rpm was quoted) from the start reaching over 500 bhp (510 bhp at 11,200 rpm was quoted) by the end of its Formula 1 career. The 1983 DFY variant had a revised bore and stroke of 90 x 59 mm (3.543 x 2.316 in) giving 2,993 cc and 520–530 bhp at 11,000 rpm, 280 ft⋅lbf (380 N⋅m) torque at 8,500 rpm.

Background

In 1965, the Fédération Internationale de l'Automobile, that administered Formula One racing, agreed to raise the series' maximum engine capacity from 1.5 litres (92 cu in) to 3.0 litres (183 cu in) from 1966. Up until that point, Colin Chapman's successful Team Lotus cars had relied on power from fast revving Coventry Climax engines, but with the change in regulations Coventry Climax decided for business reasons not to develop a large capacity engine.

Chapman approached Keith Duckworth, previously a gearbox engineer at Lotus but now running his fledgling Cosworth company with Mike Costin, who commented that he could produce a competitive three-litre engine, given a development budget of £100,000.[2]

Chapman approached the Ford Motor Company and David Brown of Aston Martin for funding, each without initial success. Chapman then approached Ford of Britain's public relations chief, former journalist Walter Hayes, with whom he had developed a close working relationship from the early 1960s. Since Hayes had joined Ford in 1962 the pair had previously collaborated in the production of the successful Lotus Cortina, introduced in 1963.[2] Hayes arranged dinner for Chapman with Ford employee Harley Copp, a British-based American engineer who had backed and engineered Ford's successful entry into NASCAR in the 1950s.[2] Hayes and Copp developed a business plan, which was backed by Ford UK's new chairman Stanley Gillen, and approved by Ford's Detroit head office as a two-part plan:

  • Stage one would produce a four-cylinder twin-cam engine for Formula Two
  • Stage two would produce a V8 engine for Formula One, by May 1967

Formula One

The project was revealed by Hayes in a PR launch in Detroit at the end of 1965, but the engine was not ready until the third race of the 1967 season, on the 4 June at Zandvoort. Its debut proved successful. Graham Hill, who was in the team at the specific request of Ford and Hayes,[2] put his DFV-powered Lotus 49 on pole position by half a second and led for the first 10 laps but was then sidelined by a broken gear in the camshaft drive. Team-mate Jim Clark moved up through the field in his identical car and came home to win. However, this dominant performance belied a serious fault in the timing gear.[3] Clark took three more wins that season, but reliability problems left him third in the Drivers' Championship, 10 points behind champion Denny Hulme. The progress of the engine was documented in a film produced by the Ford Motor Company's film section, entitled 9 Days in Summer.

Initially, the agreement between Ford, Cosworth and Lotus was binding on all parties, and Ford as the funder had no plans to sell or hire the DFV to any other teams. However, it occurred to Hayes that there was no competition: the Ferrari engine was underpowered; the BRM complex and too heavy; the Maserati unreliable; the Honda overweight; while Dan Gurney's Weslake motor was powerful but unreliable.[4] Only Brabham's Repco V8 engine provided a usable combination of power, lightness and reliability, but its age and design left little room for further improvement. Hayes concluded that Ford's name could become tarnished if the Lotus were to continue winning against only lesser opposition, and that they should agree to use the unit in other teams, and hence potentially dominate Formula One.

At the end of 1967, Copp and Hayes gently explained to Chapman that he would no longer have monopoly use of the DFV and in August 1967 it was announced that the power unit would be available for sale, via Cosworth Engineering, to racing teams throughout the world.[5] Hayes released the DFV initially to French team Matra, headed by Ken Tyrrell with Jackie Stewart as a driver. What followed was a golden age, where teams big or small could buy an engine which was competitive, light, compact, easy to work with and relatively cheap (£7,500 at 1967 prices[6] or about £90,000 in 2005 money[7]). The DFV effectively replaced the Coventry Climax as the standard F1 powerplant for the private (mostly British) teams.

Lotus, McLaren, Matra, Brabham, March, Surtees, Tyrrell, Hesketh, Lola, Williams, Penske, Wolf and Ligier are just some of the teams to have used the DFV. In 1969 and 1973 every World Championship race was won by DFV-powered cars, with the engine taking a total of 155 wins from 262 races between 1967 and 1985. The advent of ground effect aerodynamics on the F1 scene in 1977 provided a new lease of life for the now decade-old engine. The principle relied on Venturi tunnels on the underside of the car to create low pressure regions and thus additional downforce. Previously, teams running Ferrari and Alfa-Romeo flat-12 engines had enjoyed a handling advantage due to the low centre of gravity in such a configuration. However, for ground effect, the wide engine was completely the opposite of what was required as the cylinder heads protruded into the area where the Venturi tunnels should have been. In contrast, the V-configuration of the Cosworth engine angled the cylinders upwards and left ample space under the car for the necessary under-body profile[8] which massively increased downforce and gave more efficient aero balance, thus increasing cornering potential and straight line speed. Ground effect British cars and DFV engines effectively killed off the V12/flat 12 engines of Ferrari and Alfa Romeo which many pundits had believed in the mid-1970s would dominate F1 well into the mid-1980s. Drivers Mario Andretti in 1978, Alan Jones in 1980, Nelson Piquet in 1981 and Keke Rosberg in 1982 used a combination of British ground effect chassis and a DFV engine to claim the Drivers' Championship while DFV-powered cars took the Formula 1 Constructors' World Championship in 1978, 1980 and 1981.

The onset of the turbo era in the early 1980s put an end to the DFV's F1 activities, as even with modifications the 15-year-old engine could not hope to compete with the vast power being put out by the new 1.5-litre turbocharged engines. However, in the early days of turbo F1 cars (1979-1982) the Renault, Ferrari and Toleman were unable to offer consistent opposition to the Cosworth DFV British teams. The early turbo Renault, though powerful (particularly so on high altitude tracks such as Interlagos, Kyalami, Jarama, Dijon-Prenois and the Österreichring) were much heavier, cumbersome, complicated and significantly, much more unreliable than the British Cosworth DFV teams. The extra power and torque of a turbo engine put much more strain on the gearbox, driveshafts and brakes on the Renaults and Ferraris, and during the early 1980s the sight of a Renault or Ferrari wilting under the strain of its extra power was a common sight. The turbo engine was also hampered by "throttle lag", a delay in throttle response which made the turbo cars very slow on tight, twisty circuits such as Monaco, Long Beach, Zolder, Montreal, Brands Hatch and Detroit, whereas the normally-aspirated Cosworth DFV enjoyed pin-sharp response and accuracy. Also, the light and agile British cars exploited ground-effect technology so well that even on fast tracks such as Buenos Aires, Silverstone, Hockenheim the DFV engine was able to win. For a few years, between 1977 when Renault debuted the powerful but unreliable turbo engine and 1982 when the DFV-powered teams began to negotiate deals for turbo engines of their own, a competitive equilibrium was established.[9] Michele Alboreto took the DFV's last F1 win in a Tyrrell at the Detroit Grand Prix in 1983, and Martin Brundle was the last person to race in F1 with a DFV, also in a Tyrrell at the Austrian Grand Prix in 1985.

Other formulae

Sportscar racing

The DFV was used in sportscar racing with some modest success. The design of the crankshaft caused vibrations that resulted in reliability problems in endurance racing. In 1968, new rules for the Sports Prototype class limited engine displacement to 3 litres and the Cosworth DFV was available to Ford teams that year. The first such vehicle to use the DFV was the Ford P68. However, this car, and its derived sister the P69, failed to finish a single race during the two seasons that they competed. A DFV-powered Ligier JS3 was driven to a back-marker finish at Le Mans in 1971, behind a fleet of street production GT cars. The next years would show that even that unsatisfactory result was beating the odds. The DFV came into wider use in 1972, when all purpose-built racers fell under Sports Prototype rules with the 3 litre engine limit. Thirteen starts of DFV-powered vehicles at the Le Mans 24 Hours during 1972-74 yielded three finishes, two of which failed to complete 300 laps. The first win for a DFV-powered vehicle was in 1975, with the Gulf-sponsored Mirage driven by Jacky Ickx and Derek Bell. The top three finishers were powered by DFVs. The DFV-powered vehicles benefited from fuel consumption rules that had the field using low power tuning and slower engine speeds, which slowed the track pace and mitigated the DFV's vibration problem. 1976 saw a slightly faster pace for the Mirage and the DFV-powered De Cadenet Lola, but they were eclipsed by the new turbocharged Porsche 936, driven by Ickx and Gijs Van Lennep, in first place. After two years with DFV-powered vehicles failing to run competitive distances, a DFV-powered Rondeau was the surprise winner in the 1980 race. Jean Rondeau and Jean-Pierre Jaussaud nursed a two lap lead over the Jacky Ickx/Reinhold Joest Porsche 908/80 charging back from earlier mechanical setbacks. Another Rondeau occupied the third spot, nine laps behind the winner. In 1981 Rondeau slightly improved on the pace of the previous year, but as in 1976, DFV-powered vehicles were again outclassed by a Porsche 936, driven this time by the old Mirage winning team of Ickx and Bell. The 1981 distance result, 340 laps, was the best ever achieved with the DFV motor. The DFV faded from relevance over 1982-1984, showing just two finishes of over 300 laps from fourteen starts at Le Mans.

Australian race driver Bap Romano used an ex-F1 Cosworth DFV engine (formerly used by McLaren) in his Australian designed and built Kaditcha Group A Sports Car through 1983 and 1984 in the Australian Sports Car Championships. After finishing 6th in the 1983 ASCC, winning the final round of the series, he would go on to almost dominate the 1984 championship. The re-named Romano WE84 won four of the five rounds and in all bar heat two of the opening round when the car was a non-starter due to an accident in the first heat, scored fastest lap while also sitting on pole for each and every round. The DFV in the Romano was later replaced in late 1984 by the Cosworth DFL engine.

Use of post-DFV variants

1982 saw the introduction 3.3 and 3.9 litre DFLs, endurance racing versions of the DFV, in the World Sportscar Championship series. That year, the 3.3 litre variant powered two wins in the Nurburgring and Monza 1000 km events and a strong second place standing behind Porsche in season points with the new Rondeau M382. They proved insufficiently reliable for the longer events, achieving only three finishes in 34 starts at Le Mans in 1982-1984, none achieving 300 laps. After 1982 the DFLs were never reliable or competitive in the C1 class and finished consistently behind C2 cars. The 3.9 litre version was completely rejected by 1985. The last DFL to start in the C1 class at Le Mans was in 1988. 1984 saw success for the 3.3 liter version in the fuel-restricted C2 class, where low power tuning mitigated its poor reliability under a full-power setup, achieving two class wins on the World Championship circuit. The 3.3 litre DFL went on to become the most used motor of the C2 class and power four class championships, five class wins at Le Mans between 1985 and 1990, and the best distance of any Cosworth motor at Le Mans, 351 laps, in 1988. The C2 DFLs only compared favorably in reliability to the C1 DFLs, however, and as the 1980s ended the reliability issue led the FIA to seek a new formula to replace the C2 class. 1989 saw the introduction of the 3.5 litre DFZ variant as a C1 class motor. It had the honor of being the first Cosworth motor to finish ahead of the C2 winner at Le Mans, but it was an inconsistent finisher and not competitive within the C1 class. It proved a consistent finisher and winner in the FIA Cup class, the low powered equivalent of the C2 class, in 1992. The 3.5 litre DFR variant yielded more consistent results as a C1 motor for the Spice team in 1990 and the Euro Racing team in 1991, with two third-place finishes for the former, but they were never able to challenge the Peugeots, Jaguars, and Sauber Mercedes for the top spot.

Formula 3000

The DFV was also the engine for which the Formula 3000 series was created in 1985, and thus it won every race that year. The DFV and its variants continued racing in F3000 for a decade, Pedro Lamy taking the last win for a DFV in top-class motorsport, at Pau in 1993, its 65th F3000 win in 123 races.

Variants

DFW

The first variant produced from the DFV was a reduced-capacity unit for the Australia and New Zealand-based Tasman Series races of 1968–69. The changes between the DFV and DFW specification were limited to a reduced stroke, taking capacity to 2491 cc and reducing power output to ~360 bhp.[10] This was the smallest capacity variant of the DFV that was officially produced by Cosworth. The engine was a direct replacement for its DFV parent in Lotus's 49s. The small engine proved just as competitive as the larger version; and Jim Clark took four race victories in 1968, followed by one win for Piers Courage and two victories for Jochen Rindt in 1969. Derek Bell drove a DFW version of the Brabham BT26 to second place in the 1970 New Zealand Grand Prix, and for the 1971 Tasman Series previous champion Chris Amon drove a DFW-powered version of his current Formula One chassis, the March 701, to another podium finish, but in both years the Formula One-derived engine was largely outmatched by Formula 5000 entrants. After the demise of the 2.5L component of the Tasman Formula following the 1971 season, the four DFW engines were converted to DFV specification.

Formula One

The DFV had three major upgrades over its life in the top formula, with the development of first the DFY and then the DFZ, followed by a major redesign to produce the final DFR type.

DFY

With the introduction of turbocharged engines towards the end of the 1970s, Cosworth's naturally aspirated DFV began to lose its predominance. In an attempt to recover some of the performance deficit Cosworth designer Mario Illien reconfigured the cylinder aspect ratio to allow the engine to rev more freely, and combined this with a narrow-angle valve set-up and Nikasil Aluminium liners. The changes upped power output to ~520 bhp,[10] but this was not sufficient to keep pace with the turbo cars at most tracks, and it was only through a modicum of luck that Michele Alboreto was able to take what would prove to be the DFV-family's final F1 victory, at the 1983 Detroit Grand Prix. The DFY lived on with back-marker teams until the end of the 1985 season, when Cosworth switched their efforts to supporting the new turbocharged Ford GBA V6.

DFZ

The announcement at end of the 1986 season that turbocharged cars would be banned from 1989, and the introduction of the Jim Clark Cup and Colin Chapman Trophy championships for naturally aspirated cars for 1987, prompted Cosworth to revive their elderly engine design. This resulted in the DFZ, essentially an updated version of the final DFY design. However, the capacity increase for the new 3.5L naturally aspirated formula running alongside the 1.5L turbos in 1987 allowed Cosworth to increase the power output of the unit to 575 bhp (429 kW; 583 PS).[10] The engine was intended as a temporary measure to tide smaller teams over until the turbos were banned at the end of the 1988 season. Tyrrell, AGS, March, Lola and Coloni chassis were all powered by Cosworth in 1987. Jonathan Palmer of Tyrrell eventually won the drivers' Jim Clark Cup, and his team took the constructors' laurels in the Colin Chapman Trophy. The engine remained in service with minor teams until the end of 1988 and development saw a slight power increase to 590 bhp (440 kW; 598 PS). The DFZ did not race in Formula One beyond 1988 as the general release of the DFR engine made it obsolete.

The engine did however have a second brief lease of life in sportscar racing, when the FIA announced plans to transition towards using 3.5L F1-style engines in Group C in the early 1990s. In 1990 Spice Engineering adapted its existing Group C design to take a 3.5L DFZ instead of the previously used 3.3L DFL engine. However the new engine caused significant problems due to vibration, which resulted in the breakage of components and a significant increase in running costs - Gordon Spice estimated that the DFZ-powered car was about four times more expensive to run than the DFL-engined one.[11]

DFR

From 1987 Benetton had been operating as the works Ford team, essentially taking over the role from the now defunct Haas Lola team. With the abandonment of turbocharging it was clear that the venerable DFV/Y/Z design was nowhere near being competitive with far newer offerings from Honda and Renault who were building V10 engines for 1989 and beyond, and Ferrari who were building what they knew, a V12 (Lamborghini entered F1 in 1989 and like Ferrari, also went down the V12 path). To counter this, drastic changes were made for the DFR of 1988. Although superficially a DFV-design, almost the only feature carried over from previous versions into the DFR was the basic 90° V8 engine architecture. The DFR became available to all customers in 1989, with the Benetton team also using this engine until the 1989 British Grand Prix. The DFR struggled on until the 1991 season finally being eclipsed by the higher revving abilities of new pneumatic valve gear engines such as the HB, and was last used in that year's Australian Grand Prix by the Footwork, Fondmetal, Larrousse and Coloni teams, nearly a quarter of a century after the DFV's first race. By the time of its demise, continued improvement had pushed the DFR power output to nearly 630 bhp (470 kW; 639 PS),[10] 60% higher than the original 1967 DFV.

The DFR enjoyed success in 1988 with Benetton. The team was the best performed non-turbo team of the season finishing third in the Constructors' Championship behind Ferrari (turbo) and the all-conquering McLaren-Honda's. Thierry Boutsen recorded five podium finishes and Alessandro Nannini scored two podiums. The DFR was also the most powerful non-turbo of the season with a reported 620 bhp (462 kW; 629 PS). This compared to the 590 of the DFZ and the new Judd V8 with a reported 600 bhp (447 kW; 608 PS). Unfortunately this still lagged behind the Honda and Ferrari turbos which were producing over 650 bhp (485 kW; 659 PS) each.

North American series

DFX

A 2.65L turbocharged version of the DFV was developed privately by the Vels Parnelli Jones team for the 1976 USAC season, in the face of opposition from Duckworth.[12] The Parnelli-Cosworth car took its first victory at the 1976 Pocono 500, the fifth race of the season, driven by Al Unser.[12] Unser and his Cosworth-powered Parnelli took two further victories before the end of the year, in Wisconsin and Phoenix, and finished the championship in fourth position.

Duckworth had been a guest of the Vels Parnelli team during the Pocono victory, as Parnelli Jones and Vel Miletich wanted to establish the team as the North American distributor for the turbocharged, Indycar-specification engine.[12] However, shortly after the maiden race victory Cosworth poached two key engineers from the Parnelli team and set up facilities in Torrance, California, to develop and market the engine themselves.[12] Henceforth it became known as the DFX. It went on to dominate American Indy car racing in much the same way the DFV had dominated Formula One. The engine won the Indianapolis 500 ten consecutive years from 1978 until 1987, as well as winning all USAC and CART championships between 1977 and 1987 except for one. For a brief time in the early 1980s, some of the DFX engines were badged as Fords. The DFX powered 81 consecutive Indy car victories from 1981 to 1986, and 153 victories total. By the time it was replaced, the DFX was developing over 840 bhp (630 kW).[10]

DFS

In 1986 GM financed the British Ilmor firm to build a competitor to the DFX in American Indy car racing. Mario Illien's Ilmor-Chevrolet Indy V-8, which owed not a little to the DFY of five years earlier, quickly took over dominance of the sport.

Ford responded by commissioning Cosworth to redesign the DFX to include a number of DFR improvements. In 1989, they introduced an updated "short stroke" version of the Indy car engine which would be referred to as the "DFS" ("S" for short stroke).,[13] and the Nikasil Aluminium liners, adopted on DFY in 1983. The engine was fielded by two teams in its first season: Kraco Racing (Bobby Rahal) and Dick Simon Racing (Arie Luyendyk), and its development was an effort to regain dominance of the sport. At Indy, neither car qualified in the front two rows, but both started in the top ten. On race day, both drivers dropped out with engine failures. Rahal won one race in 1989 at the Meadowlands. However, the Kraco team merged with Galles at season's end, dropped the program, and switched to Chevrolets.

In 1990, the factory development was continued by Scott Brayton and Dominic Dobson,[14] but neither won any races. The engine was utilized by other CART teams in 1991–1992, and was retired after the introduction of the Ford Cosworth XB with only one victory, that being Rahal's in 1989.

DFL

In 1981 a variant of the DFV named the DFL (for long-distance) was produced specifically for use in the new Group C sports car racing class. The engine was modified to larger capacity 3,298 cc (201.3 cu in) and 3,955 cc (241.3 cu in) versions, both with wider bore and longer stroke dimensions than the standard DFV. Both versions were plagued by reliability issues worse than with the DFV they were supposed to replace. The 3.3 L version powered Rondeau to the second points standing in the World Sportscar Championship season of 1982, but it was insufficiently reliable to be competitive in the longer events. Thereafter, the 3.3 L DFL in the C1 class was unsuccessful, with those who managed to actually finish invariably ending up behind C2 cars. The new fuel-restricted C Junior (C2) class in 1983 opened a niche for successful use of the 3.3 L version, where low power tuning brought its reliability to a level where it could succeed. In the C2 category it powered many privateer cars, mostly Spices and Tigas, to class victories around the world, including five at the 24 Hours of Le Mans between 1985 and 1990. The 3.9 L version never achieved the same success as its smaller sibling, with most users finding incurable engine vibrations and it was out of competition use by 1985. It was used to power the famous Ford Supervan and Supervan 2 promotional projects, as well as the Australian designed and built Romano WE84 in the Australian Sports Car Championship, which ran the 3.0 L DFV in the championship before upgrading to the 3.9 L DFL for the 1984 World Endurance Championship round at the Sandown Raceway in Melbourne, where it finished 100 laps behind the class winner.

In August 1982, a turbocharged version of this engine was tested briefly on the Brands Hatch Circuit mounted on a Ford C100.

Major successes

DFV normally aspirated 3.0-litre 90° V8

Formula One Drivers' Champions (12):

Formula One Constructors' Champions (10):

  • 1968 Lotus
  • 1969 Matra
  • 1970 Lotus
  • 1971 Tyrrell
  • 1972 Lotus
  • 1973 Lotus
  • 1974 McLaren
  • 1978 Lotus
  • 1980 Williams
  • 1981 Williams

Le Mans 24 Hours winners (2):

Formula 3000 Champions (6):


DFX turbocharged 2.65-litre 90° V8

Indy 500 winners (10):

USAC Champions (3):

CART Champions (9):

  1. ^ The Power and the Glory: A Century of Motor Racing by Ivan Rendall Published 1991 BBC Books ISBN 0-563-36093-3
  2. ^ a b c d Ludvigsen, Karl (2007). "Walter Hayes: Racing's Ultimate Insider". Atlas F1.
  3. ^ Howard, K. (2007) Relative values. Motor Sport, 83(7), 40–43.
  4. ^ Tremayne, David (January 26, 2001). "Walter Hayes – The Father of the DFV". Grandprix.com. Retrieved December 15, 2016.
  5. ^ "Sporting side: Ford for all". Motor. nbr 3453: 57. 24 August 1968.
  6. ^ Hilton, Christopher (2002) Ken Tyrrell – Portrait of a Motor Racing Giant p38 Haynes Publishing ISBN 1-85960-885-X
  7. ^ EH.net How much is that worth today? Archived 2006-08-21 at the Wayback Machine.
  8. ^ Hughes, Mark (2004) The Unofficial Complete Encyclopedia of Formula 1, p. 55, Lorenz Books, ISBN 0-7548-1509-9
  9. ^ Hughes, Mark (2004) The Unofficial Complete Encyclopedia of Formula 1, p. 62, Lorenz Books, ISBN 0-7548-1509-9
  10. ^ a b c d e Robson, G. (2007) Cosworth DFV: Horses for courses. Motor Sport, 83(7), 44–48.
  11. ^ Cooper, Adam (24 August 2012). "The death of Group C". autosport.com. Retrieved 2 April 2016.
  12. ^ a b c d Kirby, Gordon (March 2013). "The DFX Files". Motor Sport. Vol. 89 no. 3. pp. 114–118. Retrieved 26 September 2018.
  13. ^ Glick, Shav (9 March 1989). "A Cosworth Comeback Is Key to Rahal Hopes". Los Angeles Times. Retrieved 13 October 2011.
  14. ^ Glick, Shav (24 May 1990). "11 Buicks Will Have a Race of Their Own in Indy 500". Los Angeles Times. Retrieved 13 October 2011.


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks & Buse

Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus