Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A photonics mast (or optronics mast[1]) is a sensor on a submarine which functions similarly to a periscope without requiring a periscope tube, thus freeing design space during construction and limiting risks of water leakage in the event of damage. A photonics mast replaces the mechanical, line-of-sight viewing system with digital equipment, similar to a digital camera array, and it has fewer locational and dimensional constraints than a traditional periscope.
Unlike a periscope, it need not be located directly above its user, and it requires only a small pressure hull penetration for cabling. This allows the photonics mast to fit entirely within the sail of the submarine and means the control room need not be placed directly below the sail.
A photonics mast operates by rising above the water similarly to a telescoping car-antenna and provides information through an array of sensors, such as high-definition low-light and thermographic cameras. Images and information can appear on display panels for analysis. The photonics mast can also support the navigation, electronic warfare, and communications functions of a conventional optical-periscope mast.
The Royal Navy tested an optronic mast on the Trafalgar-class HMS Trenchant in 1998. Boats of the Astute class currently under construction as of 2012[update] each have two optronic masts[1] manufactured by Thales Optronics.
In 2004, the United States Navy began fitting photonics masts to Virginia-class submarines.[2]
According to the US Navy:[3]
In Virginia-class boats, traditional periscopes have been supplanted by two Photonics Masts that house color, high-resolution black and white, and infrared digital cameras atop telescoping arms. With the removal of the barrel periscopes, the ships’ control room has been moved down one deck and away from the hull’s curvature, affording it more room and an improved layout that provides the commanding officer with enhanced situational awareness.
Wikimedia Commons has media related to Photonics masts. |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht