powered by CADENAS

Social Share

Threaded pipe (8155 views - Maschinenbau)

A threaded pipe is a pipe with screw-threaded ends for assembly.
Go to Article

Youtube


    

Threaded pipe

Threaded pipe

A threaded pipe is a pipe with screw-threaded ends for assembly.

Tapered threads

The threaded pipes used in some plumbing installations for the delivery of gases or liquids under pressure have a tapered thread that is slightly conical (in contrast to the parallel sided cylindrical section commonly found on bolts and leadscrews). The seal provided by a threaded pipe joint depends upon multiple factors: the labyrinth seal created by the threads; a positive seal between the threads created by thread deformation when they are tightened to the proper torque; and sometimes on the presence of a sealing coating, such as thread seal tape or a liquid or paste pipe sealant such as pipe dope. Tapered thread joints typically do not include a gasket.

Especially precise threads are known as "dry fit" or "dry seal" and require no sealant for a gas-tight seal. Such threads are needed where the sealant would contaminate or react with the media inside the piping, e.g., oxygen service.

Tapered threaded fittings are sometimes used on plastic piping. Due to the wedging effect of the tapered thread, extreme care must be used to avoid overtightening the joint. The overstressed female fitting may split days, weeks, or even years after initial installation. Therefore many municipal plumbing codes restrict the use of threaded plastic pipe fittings.

Both British standard and National pipe thread standards specify a thread taper of 1:16; the change in diameter is one sixteenth the distance travelled along the thread. The nominal diameter is achieved some small distance (the "gauge length") from the end of the pipe.

Straight threads

Pipes may also be threaded with cylindrical threaded sections, in which case the threads do not themselves provide any sealing function other than some labyrinth seal effect, which may not be enough to satisfy either functional or code requirements. Instead, an O-ring seated between the shoulder of the male pipe section and an interior surface on the female, provides the seal.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Maschinenbau

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD