Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 3.0 (Diego Delso ).
what are the Niagara falls? The Niagara Fall consists of three waterfalls including the Canadian Horseshoe Falls, American Falls and Bridal Veil Falls.
Bridal Veil Falls is the smallest among the others, flowing approximately 567, 811 litres per second and stands at the height of roughly fifty meters. Canadian “Horseshoe” Falls flows about 2,271,247 litres per second, which is the most water among the other Falls. It stands at the height of approximately 50.9 meters. While it stands at about 56 meters, the estimated flow of American Falls is between 500,00 to 1,00,00 litres.
A waterfall is an area where water flows over a vertical drop or a series of steep drops in the course of a stream or river. Waterfalls also occur where meltwater drops over the edge of a tabular iceberg or ice shelf.
Waterfalls are commonly formed in the upper course of a river in steep mountains.[1] Because of their landscape position, many waterfalls occur over bedrock fed by little contributing area, so may be ephemeral and flow only during rainstorms or significant snowmelt. The further downstream, the more perennial a waterfall can be. Waterfalls can have a wide range of widths and depths.
When the river courses over resistant bedrock, erosion happens slowly and is dominated by impacts of water-borne sediment on the rock, while downstream the erosion occurs more rapidly.[1][3] As the watercourse increases its velocity at the edge of the waterfall, it may pluck material from the riverbed, if the bed is fractured or otherwise more erodible. Hydraulic jets and hydraulic jumps at the toe of a falls can generate large forces to erode the bed,[4] especially when forces are amplified by water-borne sediment. Horseshoe-shaped falls focus the erosion to a central point, also enhancing riverbed change below a waterfalls.[5] A process known as "potholing" involves local erosion of a potentially deep hole in bedrock due to turbulent whirlpools spinning stones around on the bed, drilling it out. Sand and stones carried by the watercourse therefore increase erosion capacity.[1] This causes the waterfall to carve deeper into the bed and to recede upstream. Often over time, the waterfall will recede back to form a canyon or gorge downstream as it recedes upstream, and it will carve deeper into the ridge above it.[6] The rate of retreat for a waterfall can be as high as one-and-a-half metres per year.[1]
Often, the rock stratum just below the more resistant shelf will be of a softer type, meaning that undercutting due to splashback will occur here to form a shallow cave-like formation known as a rock shelter under and behind the waterfall. Eventually, the outcropping, more resistant cap rock will collapse under pressure to add blocks of rock to the base of the waterfall. These blocks of rock are then broken down into smaller boulders by attrition as they collide with each other, and they also erode the base of the waterfall by abrasion, creating a deep plunge pool in the gorge downstream.
Streams can become wider and shallower just above waterfalls due to flowing over the rock shelf, and there is usually a deep area just below the waterfall because of the kinetic energy of the water hitting the bottom. However, a study of waterfalls systematics reported that waterfalls can be wider or narrower above or below a falls, so almost anything is possible given the right geological and hydrological setting.[7] Waterfalls normally form in a rocky area due to erosion. After a long period of being fully formed, the water falling off the ledge will retreat, causing a horizontal pit parallel to the waterfall wall. Eventually, as the pit grows deeper, the waterfall collapses to be replaced by a steeply sloping stretch of river bed.[1] In addition to gradual processes such as erosion, earth movement caused by earthquakes or landslides or volcanoes can cause a differential in land heights which interfere with the natural course of a water flow, and result in waterfalls.
A river sometimes flows over a large step in the rocks that may have been formed by a fault line. Waterfalls can occur along the edge of a glacial trough, where a stream or river flowing into a glacier continues to flow into a valley after the glacier has receded or melted. The large waterfalls in Yosemite Valley are examples of this phenomenon, which is referred to as a hanging valley. Another reason hanging valleys may form is where two rivers join and one is flowing faster than the other.[1]
Waterfalls can be grouped into ten broad classes based on the average volume of water present on the fall (which depends on both the waterfall's average flow and its height) using a logarithmic scale. Class 10 waterfalls include Niagara Falls, Paulo Afonso Falls and Khone Falls.
Classes of other well-known waterfalls include Victoria Falls and Kaieteur Falls (Class 9); Rhine Falls and Gullfoss (Class 8); Angel Falls and Dettifoss (Class 7); Yosemite Falls, Lower Yellowstone Falls, and Umphang Thee Lor Sue Waterfall (Class 6); and Sutherland Falls (Class 5).[8]
Alexander von Humboldt (1820s) "Father of Modern Geography" Humboldt was mostly marking waterfalls on maps for river navigation purposes.
Oscar von Engeln (1930s) Published "Geomorphology: systematic and regional", this book had a whole chapter devoted to waterfalls, and is one of the earliest examples of published works on waterfalls.
R. W. Young (1980s) Wrote "Waterfalls: form and process" this work made waterfalls a much more serious topic for research for modern Geoscientists.[9]
Some waterfalls are also distinct in that they do not flow continuously. Ephemeral waterfalls only flow after a rain or a significant snowmelt.[11][12][13]
Aerial view of Iguazu Falls on the Iguazu River between Brazil and Argentina.
Aerial view of Niagara Falls in the state of New York, United States, and province of Ontario, Canada.
Nohkalikai Falls is one of the tallest plunge type waterfalls in India.[14]
Staubbach Falls, a 297-metre (974 ft) waterfall in Switzerland.
Significant waterfalls,[15] listed alphabetically:
Huangguoshu Waterfall in Guizhou province, China, is a block-type waterfall and a cataract.
Song Khon Waterfall in Loei Province, Thailand is an example of a cascade waterfall.
In Pamukkale, Turkey is an example of travertine terraces built by flowing water.
First fall of Elephant Falls in Shillong, India, is an example of a horsetail-punchbowl waterfall.
Wikimedia Commons has media related to Waterfall. |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,model,rendering,library,tree,bush,flower,landscape,design,architecure,plant