powered by CADENAS

Social Share

Threaded insert (15183 views - Maschinenbau)

A threaded insert, also known as a threaded bushing, is a fastener element that is inserted into an object to add a threaded hole. They may be used to repair a stripped threaded hole, provide a durable threaded hole in a soft material, place a thread on a material too thin to accept it, mold or cast threads into a work piece thereby eliminating a machining operation, or simplify changeover from unified to metric threads or vice versa.
Go to Article

Threaded insert

Threaded insert

A threaded insert, also known as a threaded bushing, is a fastener element that is inserted into an object to add a threaded hole.[1] They may be used to repair a stripped threaded hole, provide a durable threaded hole in a soft material, place a thread on a material too thin to accept it, mold or cast threads into a work piece thereby eliminating a machining operation, or simplify changeover from unified to metric threads or vice versa.[2]

Types

Thread inserts come in many varieties, depending on the application. Threaded inserts for plastics are used in plastic materials and applied with thermal insertion or ultrasonic welding machines.

Manufacturers of knock-down furniture often ship the parts with threaded inserts and other kinds of knock-down fasteners pre-installed.

People who use sheet metal or sandwich panel or honeycomb sandwich-structured composite often install threaded inserts to spread shear, tension, and torque loads over a larger area of the material.[3]

Captive nut

Captive nuts come in two basic styles. One type, the cage nut or clip-on nut is a conventional nut held captive by a sheet metal carrier that clips onto the part to be connected. These are generally used to attach screws to sheet metal parts too thin to be threaded, and they can generally be attached, removed and reused with simple hand tools.

The second type of captive nut is a threaded insert. These are either pressed into holes in the material to be joined or moulded in. In either case, part of the insert is generally knurled to get a good grip on the material supporting the insert. One variant, the swage nut, has a knurled portion that swages the sides of a soft metal hole to more tightly grip the nut. Press fit and swaged captive nuts are used in panels that are too thin to be threaded or in soft materials that are too weak to be threaded. They are installed by pressing them in with an arbor press.[4]

Threaded inserts are commonly used in plastic casings, housing, and parts to create a metal thread (typically: Brass or Stainless Steel) to allow for screws to be used in the assembly of many consumer electronics and consumer products. These may be cast in place in injection molded parts or they may be added by thermal insertion. In the latter, the insert is heated and then pressed into a hollow in the plastic part. The heat causes local melting in the plastic.[5] Ultrasonic Insertion is the process used to apply vibration and pressure to install the threaded insert into a molded hollow boss (hole) of a plastic part. The ultrasonic vibrations melt the plastic where the metal insert is in contact, and pressure is applied to press it into position. The plastic material typically reforms around the knurled body of the threaded insert to ensure a good retention.

Externally-threaded inserts

Externally threaded inserts have threads on the outside and inside of the insert. The insert is threaded into a pre-tapped hole, or some inserts tap their own threads in a drilled or molded hole. It is then anchored by various means, such as a nylon locking element. Inserts that are anchored via Loctite are more commonly known by the trademarked name E-Z Lok.[6] A thin walled solid bushing insert by the trademarked name TIME-SERT is locked in by rolling the bottom few internal thread into the base material with a special install driver which will permanently lock the insert in place.[citation needed] Key locking inserts, more commonly known by the trademarked name Keenserts, use keys that are hammered into grooves through the threads, permanently locking the insert.[7][8][9] Inserts that are self-tapping and lock via friction are more commonly known by the trademarked names Tap-lok or Speedserts.

Helical insert

A helical insert is an insert made of coiled wire. The helically formed coils of diamond shaped stainless steel or phosphor bronze wire screw into a threaded hole to form a mating internal thread for a screw or stud. These inserts provide a convenient means of repairing stripped-out threads and are also used to provide stronger threads in soft materials such as aluminium, zinc die castings, wood, magnesium etc. than can be obtained by direct tapping of the base metal involved. Another common generic name is screw thread insert (STI), although many users persist in calling them all by a prominent brand name, the registered trademark Heli-Coil. Applications include engine cylinder head repair after unintentional over-torquing or cross-threading of spark plugs strips the thread of the socket. Kits with matched tap and coil exist for this. The straight radial piece in the photo is the driver tang which is used as a key to grip with pliers for driving the coil into place and is discarded after installation.

Mold-in inserts

Mold-in inserts are internally threaded and have a specially shaped outer diameter to anchor the insert in plastic. The insert is placed in the mold of an injection molded part beforehand. The mold is then closed and filled with the plastic filling in around the insert. These inserts can also be heated and pressed into pre-made thermoplastics.[10]

For softer more pliable plastics, hexagonal or square inserts with deep and wide grooves allow the plastic to flow and adhere. The process allows large product manufacture i.e. fuel tanks, boats etc., so the torque inserts may be of large thread sizes.

Press fit inserts

Press fit inserts are internally threaded and have a knurled outer diameter. They are pressed into a plain hole with an arbor press.[10]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Example Part

Maschinenbau

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD