powered by CADENAS

Social Share

Amazon

Arbor press (9397 views - Maschinenbau)

An arbor press is a small hand operated press. It is typically used to perform smaller jobs, such as staking, riveting, installing, configuring and removing bearings and other press fit work. Punches, inserters, or other tools/dies may be added to the end of the ram depending on the desired task. Arbor presses are usually rated by the maximum load they can apply. Typically common are presses with a leverage of 1–5 tons. This leverage is achieved when a force is applied to the lever arm or wheel. Arbor presses can be mounted on a work bench, wall, or pedestal. The base is usually constructed of cast metal. A ram provides the force; it may be square or round. The ram is usually driven by a rack and pinion setup, to improve the mechanical advantage. Higher force arbor presses have another gear reduction. Forces are usually generated by manual or hydraulic input.
Go to Article

Explanation by Hotspot Model

Arbor press

Arbor press

An arbor press is a small hand operated press. It is typically used to perform smaller jobs, such as staking, riveting, installing, configuring and removing bearings and other press fit work. Punches, inserters, or other tools/dies may be added to the end of the ram depending on the desired task. Arbor presses are usually rated by the maximum load they can apply.[1] Typically common are presses with a leverage of 1–5 tons. This leverage is achieved when a force is applied to the lever arm or wheel.

Arbor presses can be mounted on a work bench, wall, or pedestal. The base is usually constructed of cast metal. A ram provides the force; it may be square or round. The ram is usually driven by a rack and pinion setup, to improve the mechanical advantage. Higher force arbor presses have another gear reduction.[1] Forces are usually generated by manual or hydraulic input.[2]

  1. ^ a b McMaster-Carr, catalog page 2269. 2269.
  2. ^ US 3686922 

Bibliography

  • "McMaster-Carr catalog" (114th ed.). McMaster-Carr. 




This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Maschinenbau

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD