powered by CADENAS

Social Share

Pipe wrench (11779 views - Tooling)

The pipe wrench (US), Stillson wrench or Stillsons (UK) is an adjustable wrench/spanner used for turning soft iron pipes and fittings with a rounded surface. The design of the adjustable jaw allows it to lock in the frame, such that any forward pressure on the handle tends to pull the jaws tighter together. Teeth angled in the direction of turn dig into the soft pipe. They are not intended for use on hardened steel hex nuts or other fittings because they would ruin the head; however, if a hex nut is soft enough that it becomes rounded beyond use with standard wrenches, a pipe wrench is sometimes used to break the bolt or nut free. Pipe wrenches are usually sold in the following sizes (by length of handle): 10, 12, 14, 18, 24, 36, and 48 inches, although smaller and larger sizes are available as well. They are usually made of cast steel. Today, aluminium is also used to construct the body of the wrench, while the teeth and jaw remain steel. Teeth, and jaw kits (which also contain adjustment rings and springs) can be bought to repair broken wrenches, as this is cheaper than buying a new wrench.
Go to Article

Explanation by Hotspot Model

Pipe wrench

Pipe wrench

Pipe wrench
A modern pipe wrench.
Classification hand tool
Related wrench, plumber wrench, monkey wrench

The pipe wrench (US), Stillson wrench or Stillsons (UK) is an adjustable wrench/spanner used for turning soft iron pipes and fittings with a rounded surface. The design of the adjustable jaw allows it to lock in the frame, such that any forward pressure on the handle tends to pull the jaws tighter together. Teeth angled in the direction of turn dig into the soft pipe. They are not intended for use on hardened steel hex nuts or other fittings because they would ruin the head; however, if a hex nut is soft enough that it becomes rounded beyond use with standard wrenches, a pipe wrench is sometimes used to break the bolt or nut free. Pipe wrenches are usually sold in the following sizes (by length of handle): 10, 12, 14, 18, 24, 36, and 48 inches, although smaller and larger sizes are available as well. They are usually made of cast steel. Today, aluminium is also used to construct the body of the wrench, while the teeth and jaw remain steel. Teeth, and jaw kits (which also contain adjustment rings and springs) can be bought to repair broken wrenches, as this is cheaper than buying a new wrench.

History

The first pipe, or stillson, wrench was created by Daniel C. Stillson (1826-1899) while working as a mechanic at the Walworth Company, in Cambridge, Massachusetts.[1] On October 12, 1869, U.S. patent #95,744 was issued to Stillson.[2]

In Prince Edward Island, Canada there is some controversy over the true creator of the wrench. In the island folklore, the wrench was developed by Owen "Iney" McCluskey, although no proof has ever been presented that would suggest that McCluskey and Stillson ever met.

On 17 August 1888 the Swedish inventor Johan Petter Johansson (1853-1943) took his first patent on the adjustable pipe wrench.[3] The Swedish Patent Office issued the patent (SE 5636) again in 1894. The idea emerged after he established his company Enköpings Mekaniska Verkstad. Back then there was no standard on nut dimensions so each time a trades man was out on a job, he needed a trolley to take a whole set of fixed pipe wrenches with him. Johan Petter Johansson invented a tool that could grip nuts of different dimensions.[4]

Pipe wrench in different countries

In South Africa, the terms "bobbejaan spanner" and "baboon spanner" are commonly used,[5] especially for large pipe wrenches. "Bobbejaan" is the Afrikaans term for a baboon. In Zimbabwe it was usually known by an Anglicized version of the Afrikaans name, "bobbiejohn spanner".

In the United Kingdom these wrenches are often described by their size, i.e. 18" wrenches are known as "18s", or by the general name of "Stillies/stills".[citation needed]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing