powered by CADENAS

Social Share

Technetium (21375 views - Periodic Table Of Elements)

Technetium is a chemical element with symbol Tc and atomic number 43. It is the lightest element whose isotopes are all radioactive; none are stable. Nearly all technetium is produced synthetically, and only minute amounts are found in the Earth's crust. Naturally occurring technetium is a spontaneous fission product in uranium ore or the product of neutron capture in molybdenum ores. The chemical properties of this silvery gray, crystalline transition metal are intermediate between rhenium and manganese. Many of technetium's properties were predicted by Dmitri Mendeleev before the element was discovered. Mendeleev noted a gap in his periodic table and gave the undiscovered element the provisional name ekamanganese (Em). In 1937, technetium (specifically the technetium-97 isotope) became the first predominantly artificial element to be produced, hence its name (from the Greek τεχνητός, meaning "artificial", + -ium). One short-lived gamma ray-emitting nuclear isomer of technetium—technetium-99m—is used in nuclear medicine for a wide variety of diagnostic tests. The ground state of this nuclide, technetium-99, is used as a gamma-ray-free source of beta particles. Long-lived technetium isotopes produced commercially are by-products of the fission of uranium-235 in nuclear reactors and are extracted from nuclear fuel rods. Because no isotope of technetium has a half-life longer than 4.2 million years (technetium-98), the 1952 detection of technetium in red giants, which are billions of years old, helped to prove that stars can produce heavier elements.
Go to Article

Technetium

Technetium

Technetium,  43Tc
General properties
Pronunciation /tɛkˈnʃiəm/
tek-NEE-shee-əm
Appearance shiny gray metal
Mass number 98 (most stable isotope)
Technetium in the periodic table
Mn

Tc

Re
molybdenumtechnetiumruthenium
Atomic number (Z) 43
Group, period group 7, period 5
Block d-block
Element category   transition metal
Electron configuration [Kr] 4d5 5s2
Electrons per shell
2, 8, 18, 13, 2
Physical properties
Spectral lines
Phase (at STP) solid
Melting point 2430 K ​(2157 °C, ​3915 °F)
Boiling point 4538 K ​(4265 °C, ​7709 °F)
Density (near r.t.) 11 g/cm3
Heat of fusion 33.29 kJ/mol
Heat of vaporization 585.2 kJ/mol
Molar heat capacity 24.27 J/(mol·K)
Vapor pressure (extrapolated)
P (Pa) 1 10 100 1 k 10 k 100 k
at T (K) 2727 2998 3324 3726 4234 4894
Atomic properties
Oxidation states 7, 6, 5, 4, 3,[1] 2, 1,[1] −1, −3 ​(a strongly acidic oxide)
Electronegativity Pauling scale: 1.9
Ionization energies
  • 1st: 702 kJ/mol
  • 2nd: 1470 kJ/mol
  • 3rd: 2850 kJ/mol
Atomic radius empirical: 136 pm
Covalent radius 147±7 pm
Miscellanea
Crystal structurehexagonal close-packed (hcp)
Speed of sound thin rod 16,200 m/s (at 20 °C)
Thermal expansion 7.1 µm/(m·K)[2] (at r.t.)
Thermal conductivity 50.6 W/(m·K)
Electrical resistivity 200 nΩ·m (at 20 °C)
Magnetic ordering Paramagnetic
Magnetic susceptibility +270.0·10−6 cm3/mol (298 K)[3]
CAS Number 7440-26-8
History
Prediction Dmitri Mendeleev (1871)
Discovery and first isolation Emilio Segrè and Carlo Perrier (1937)
Main isotopes of technetium
Iso­tope Abun­dance Half-life (t1/2) Decay mode Pro­duct
95mTc syn 61 d ε 95Mo
γ
IT 95Tc
96Tc syn 4.3 d ε 96Mo
γ
97Tc syn 2.6×106 y ε 97Mo
97mTc syn 91 d IT 97Tc
98Tc syn 4.2×106 y β 98Ru
γ
99Tc trace 2.111×105 y β 99Ru
99mTc syn 6.01 h IT 99Tc
γ
| references | in Wikidata

Technetium is a chemical element with symbol Tc and atomic number 43. It is the lightest element whose isotopes are all radioactive; none are stable. Nearly all technetium is produced synthetically, and only minute amounts are found in the Earth's crust. Naturally occurring technetium is a spontaneous fission product in uranium ore or the product of neutron capture in molybdenum ores. The chemical properties of this silvery gray, crystalline transition metal are intermediate between rhenium and manganese.

Many of technetium's properties were predicted by Dmitri Mendeleev before the element was discovered. Mendeleev noted a gap in his periodic table and gave the undiscovered element the provisional name ekamanganese (Em). In 1937, technetium (specifically the technetium-97 isotope) became the first predominantly artificial element to be produced, hence its name (from the Greek τεχνητός, meaning "artificial", + -ium).

One short-lived gamma ray-emitting nuclear isomer of technetium—technetium-99m—is used in nuclear medicine for a wide variety of diagnostic tests. The ground state of this nuclide, technetium-99, is used as a gamma-ray-free source of beta particles. Long-lived technetium isotopes produced commercially are by-products of the fission of uranium-235 in nuclear reactors and are extracted from nuclear fuel rods. Because no isotope of technetium has a half-life longer than 4.2 million years (technetium-98), the 1952 detection of technetium in red giants, which are billions of years old, helped to prove that stars can produce heavier elements.

History

Search for element 43

From the 1860s through 1871, early forms of the periodic table proposed by Dmitri Mendeleev contained a gap between molybdenum (element 42) and ruthenium (element 44). In 1871, Mendeleev predicted this missing element would occupy the empty place below manganese and have similar chemical properties. Mendeleev gave it the provisional name ekamanganese (from eka-, the Sanskrit word for one) because the predicted element was one place down from the known element manganese.[4]

Early misidentifications

Many early researchers, both before and after the periodic table was published, were eager to be the first to discover and name the missing element. Its location in the table suggested that it should be easier to find than other undiscovered elements.

Year Claimant Suggested name Actual material
1828 Gottfried Osann Polinium Iridium
1846 R. Hermann Ilmenium Niobium-tantalum alloy
1847 Heinrich Rose Pelopium[5] Niobium-tantalum alloy
1877 Serge Kern Davyum Iridium-rhodium-iron alloy
1896 Prosper Barrière Lucium Yttrium
1908 Masataka Ogawa Nipponium Rhenium, which was the then unknown dvi-manganese[6]

Irreproducible results

Periodisches System der Elemente (1904–1945, now at the Gdańsk University of Technology): lack of elements: 84 polonium Po (though discovered as early as in 1898 by Maria Sklodowska-Curie), 85 astatine At (1940, in Berkeley), 87 francium Fr (1939, in France), 93 neptunium Np (1940, in Berkeley) and other actinides and lanthanides. Old symbols for: 18 argon Ar (here: A), 43 technetium Tc (Ma, masurium, 1925, dismissed as an error and finally confirmed in 1937, Palermo), 54 xenon Xe (X), 86 radon, Rn (Em, emanation)

German chemists Walter Noddack, Otto Berg, and Ida Tacke reported the discovery of element 75 and element 43 in 1925, and named element 43 masurium (after Masuria in eastern Prussia, now in Poland, the region where Walter Noddack's family originated).[7] The group bombarded columbite with a beam of electrons and deduced element 43 was present by examining X-ray diffraction spectrograms.[8] The wavelength of the X-rays produced is related to the atomic number by a formula derived by Henry Moseley in 1913. The team claimed to detect a faint X-ray signal at a wavelength produced by element 43. Later experimenters could not replicate the discovery, and it was dismissed as an error for many years.[9][10] Still, in 1933, a series of articles on the discovery of elements quoted the name masurium for element 43.[11][note 1] Whether the 1925 team actually did discover element 43 is still debated.[12]

Official discovery and later history

The discovery of element 43 was finally confirmed in a December 1936 experiment at the University of Palermo in Sicily by Carlo Perrier and Emilio Segrè.[13] In mid-1936, Segrè visited the United States, first Columbia University in New York and then the Lawrence Berkeley National Laboratory in California. He persuaded cyclotron inventor Ernest Lawrence to let him take back some discarded cyclotron parts that had become radioactive. Lawrence mailed him a molybdenum foil that had been part of the deflector in the cyclotron.[14]

Segrè enlisted his colleague Perrier to attempt to prove, through comparative chemistry, that the molybdenum activity was indeed from an element with the atomic number 43. In 1937 they succeeded in isolating the isotopes technetium-95m and technetium-97.[15][16] University of Palermo officials wanted them to name their discovery "panormium", after the Latin name for Palermo, Panormus. In 1947[15] element 43 was named after the Greek word τεχνητός, meaning "artificial", since it was the first element to be artificially produced.[5][7] Segrè returned to Berkeley and met Glenn T. Seaborg. They isolated the metastable isotope technetium-99m, which is now used in some ten million medical diagnostic procedures annually.[17]

In 1952, astronomer Paul W. Merrill in California detected the spectral signature of technetium (specifically wavelengths of 403.1 nm, 423.8 nm, 426.2 nm, and 429.7 nm) in light from S-type red giants.[18] The stars were near the end of their lives, yet were rich in this short-lived element, indicating that it was being produced in the stars by nuclear reactions. This evidence bolstered the hypothesis that heavier elements are the product of nucleosynthesis in stars.[16] More recently, such observations provided evidence that elements are formed by neutron capture in the s-process.[19]

Since that discovery, there have been many searches in terrestrial materials for natural sources of technetium. In 1962, technetium-99 was isolated and identified in pitchblende from the Belgian Congo in extremely small quantities (about 0.2 ng/kg);[19] there it originates as a spontaneous fission product of uranium-238. The Oklo natural nuclear fission reactor contains evidence that significant amounts of technetium-99 were produced and have since decayed into ruthenium-99.[19]

Characteristics

Physical properties

Technetium is a silvery-gray radioactive metal with an appearance similar to platinum, commonly obtained as a gray powder.[20] The crystal structure of the pure metal is hexagonal close-packed. Atomic technetium has characteristic emission lines at these wavelengths of light: 363.3 nm, 403.1 nm, 426.2 nm, 429.7 nm, and 485.3 nm.[21]

The metal form is slightly paramagnetic, meaning its magnetic dipoles align with external magnetic fields, but will assume random orientations once the field is removed.[22] Pure, metallic, single-crystal technetium becomes a type-II superconductor at temperatures below 7.46 K.[note 2][23] Below this temperature, technetium has a very high magnetic penetration depth, greater than any other element except niobium.[24]

Chemical properties

Technetium is located in the seventh group of the periodic table, between rhenium and manganese. As predicted by the periodic law, its chemical properties are between those two elements. Of the two, technetium more closely resembles rhenium, particularly in its chemical inertness and tendency to form covalent bonds.[25] Unlike manganese, technetium does not readily form cations (ions with a net positive charge). Technetium exhibits nine oxidation states from −1 to +7, with +4, +5, and +7 being the most common.[26] Technetium dissolves in aqua regia, nitric acid, and concentrated sulfuric acid, but it is not soluble in hydrochloric acid of any concentration.[20]

Metallic technetium slowly tarnishes in moist air[26] and, in powder form, burns in oxygen.

Technetium can catalyse the destruction of hydrazine by nitric acid, and this property is due to its multiplicity of valencies.[27] This caused a problem in the separation of plutonium from uranium in nuclear fuel processing, where hydrazine is used as a protective reductant to keep plutonium in the trivalent rather than the more stable tetravalent state. The problem was exacerbated by the mutually-enhanced solvent extraction of technetium and zirconium at the previous stage,[28] and required a process modification.

Compounds

Pertechnetate and derivatives

Pertechnetate is one of the most available forms of technetium. It is structurally related to permanganate.

The most prevalent form of technetium that is easily accessible is sodium pertechnetate, Na[TcO4]. The majority of this material is produced by radioactive decay from [99MoO4]2−:[29][30]

[99MoO4]2− → [99TcO4] + γ

Pertechnetate (tetroxidotechnetate) TcO
4
behaves analogously to perchlorate, with which it is isostructural. It is tetrahedral. Unlike permanganate (MnO
4
), it is only a weak oxidizing agent.

Related to pertechnetate is heptoxide. This pale-yellow, volatile solid is produced by oxidation of Tc metal and related precursors:

4 Tc + 7 O2 → 2 Tc2O7

It is a very rare example of a molecular metal oxide, other examples being OsO4 and RuO4. It adopts a centrosymmetric structure with two types of Tc−O bonds with 167 and 184 pm bond lengths.[31]

Technetium heptoxide hydrolyzes to pertechnetate and pertechnetic acid, depending on the pH:[32]

[33]
Tc2O7 + 2 OH → 2 TcO4 + H2O
Tc2O7 + H2O → 2 HTcO4

Dark red, hygroscopic HTcO4 is a strong acid. In concentrated sulfuric acid, [TcO4] converts to the octahedral form TcO3(OH)(H2O)2, the conjugate base of the hypothetical triaquo complex [TcO3(H2O)3]+.[34]

Other chalcogenide derivatives

Technetium forms a dioxide,[35] disulfide, diselenide, and ditelluride. An ill-defined Tc2S7 forms upon treating pertechnate with hydrogen sulfide. It thermally decomposes into disulfide and elemental sulfur.[36] Similarly the dioxide can be produced by reduction of the Tc2O7.

Unlike the case for rhenium, a trioxide has not been isolated for Tc. However, TcO3 has been identified in the gas phase using mass spectrometry.[37]

Simple hydride and halide complexes

Technetium forms the simple complex TcH2−
9
. The potassium salt is isostructural with ReH2−
9
.[38]

The following binary (containing only two elements) technetium halides are known: TcF6, TcF5, TcCl4, TcBr4, TcBr3, α-TcCl3, β-TcCl3, TcI3, α-TcCl2, and β-TcCl2. The oxidation states range from Tc(VI) to Tc(II). Technetium halides exhibit different structure types, such as molecular octahedral complexes, extended chains, layered sheets, and metal clusters arranged in a three-dimensional network.[39][40] These compounds are produced by combining the metal and halogen or by less direct reactions.

TcCl4 is obtained by chlorination of Tc metal or Tc2O7 Upon heating, TcCl4 gives the corresponding Tc(III) and Tc(II) chlorides.[40]

TcCl4 → α-TcCl3 + 1/2 Cl2
TcCl3 → β-TcCl2 + 1/2 Cl2
TcCl4 forms chain-like structures, similar to the behavior of several other metal tetrachlorides.

The structure of TcCl4 is composed of infinite zigzag chains of edge-sharing TcCl6 octahedra. It is isomorphous to transition metal tetrachlorides of zirconium, hafnium, and platinum.[40]

Two polymorphs of technetium trichloride exist, α- and β-TcCl3. The α polymorph is also denoted as Tc3Cl9. It adopts a confacial bioctahedral structure.[41] It is prepared by treating the chloro-acetate Tc2(O2CCH3)4Cl2 with HCl. Like Re3Cl9, the structure of the α-polymorph consists of triangles with short M-M distances. β-TcCl3 features octahedral Tc centers, which are organized in pairs, as seen also for molybdenum trichloride. TcBr3 does not adopt the structure of either trichloride phase. Instead it has the structure of molybdenum tribromide, consisting of chains of confacial octahedra with alternating short and long Tc—Tc contacts. TcI3 has the same structure as the high temperature phase of TiI3, featuring chains of confacial octahedra with equal Tc—Tc contacts.[40]

Several anionic technetium halides are known. The binary tetrahalides can be converted to the hexahalides [TcX6]2− (X = F, Cl, Br, I), which adopt octahedral molecular geometry.[19] More reduced halides form anionic clusters with Tc-Tc bonds. The situation is similar for the related elements of Mo, W, Re. These clusters have the nuclearity Tc4, Tc6, Tc8, and Tc13. The more stable Tc6 and Tc8 clusters have prism shapes where vertical pairs of Tc atoms are connected by triple bonds and the planar atoms by single bonds. Every technetium atom makes six bonds, and the remaining valence electrons can be saturated by one axial and two bridging ligand halogen atoms such as chlorine or bromine.[42]

Coordination and organometallic complexes

Technetium forms a variety of coordination complexes with organic ligands. Many have been well-investigated because of their relevance to nuclear medicine.[43]

Technetium forms a variety of compounds with Tc–C bonds, i.e. organotechnetium complexes. Prominent members of this class are complexes with CO, arene, and cyclopentadienyl ligands.[44] The binary carbonyl Tc2(CO)10 is a white volatile solid.[45] In this molecule, two technetium atoms are bound to each other; each atom is surrounded by octahedra of five carbonyl ligands. The bond length between technetium atoms, 303 pm,[46][47] is significantly larger than the distance between two atoms in metallic technetium (272 pm). Similar carbonyls are formed by technetium's congeners, manganese and rhenium.[48] Interest in organotechnetium compounds has also been motivated by applications in nuclear medicine.[44] Unusual for other metal carbonyls, Tc forms aquo-carbonyl complexes, prominent being [Tc(CO)3(H2O)3]+.[44]

Isotopes

Technetium, with atomic number (denoted Z) 43, is the lowest-numbered element in the periodic table of which all isotopes are radioactive. The second-lightest exclusively radioactive element, promethium, has an atomic number of 61.[26] Atomic nuclei with an odd number of protons are less stable than those with even numbers, even when the total number of nucleons (protons + neutrons) is even,[49] and odd numbered elements have fewer stable isotopes.

The most stable radioactive isotopes are technetium-98 with a half-life of 4.2 million years (Ma), technetium-97 with 2.6 Ma, and technetium-99 with 211,000 years.[50] Thirty other radioisotopes have been characterized with mass numbers ranging from 85 to 118.[50] Most of these have half-lives that are less than an hour, the exceptions being technetium-93 (half-life: 2.73 hours), technetium-94 (half-life: 4.88 hours), technetium-95 (half-life: 20 hours), and technetium-96 (half-life: 4.3 days).[51]

The primary decay mode for isotopes lighter than technetium-98 (98Tc) is electron capture, producing molybdenum (Z = 42).[50] For technetium-98 and heavier isotopes, the primary mode is beta emission (the emission of an electron or positron), producing ruthenium (Z = 44), with the exception that technetium-100 can decay both by beta emission and electron capture.[50][52]

Technetium also has numerous nuclear isomers, which are isotopes with one or more excited nucleons. Technetium-97m (97mTc; 'm' stands for metastability) is the most stable, with a half-life of 91 days (0.0965 MeV).[51] This is followed by technetium-95m (half-life: 61 days, 0.03 MeV), and technetium-99m (half-life: 6.01 hours, 0.142 MeV).[51] Technetium-99m emits only gamma rays and decays to technetium-99.[51]

Technetium-99 (99Tc) is a major product of the fission of uranium-235 (235U), making it the most common and most readily available isotope of technetium. One gram of technetium-99 produces 6.2×108 disintegrations a second (that is, 0.62 GBq/g).[22]

Occurrence and production

Only minute traces of technetium occur naturally in the Earth's crust. This is because technetium-98's half-life is only 4.2 million years. More than a thousand of such periods have passed since the formation of the Earth, so the probability for the survival of even one atom of primordial technetium is effectively zero. However, small amounts exist as spontaneous fission products in uranium ores. A kilogram of uranium contains an estimated 1 nanogram (10−9 g) of technetium.[16][53][54] Some red giant stars with the spectral types S-, M-, and N contain a spectral absorption line indicating the presence of technetium.[20][55] These red-giants are known informally as technetium stars.

Fission waste product

In contrast to the rare natural occurrence, bulk quantities of technetium-99 are produced each year from spent nuclear fuel rods, which contain various fission products. The fission of a gram of uranium-235 in nuclear reactors yields 27 mg of technetium-99, giving technetium a fission product yield of 6.1%.[22] Other fissile isotopes produce similar yields of technetium, such as 4.9% from uranium-233 and 6.21% from plutonium-239.[56] An estimated 49,000 TBq (78 metric tons) of technetium was produced in nuclear reactors between 1983 and 1994, by far the dominant source of terrestrial technetium.[57][58] Only a fraction of the production is used commercially.[note 3]

Technetium-99 is produced by the nuclear fission of both uranium-235 and plutonium-239. It is therefore present in radioactive waste and in the nuclear fallout of fission bomb explosions. Its decay, measured in becquerels per amount of spent fuel, is the dominant contributor to nuclear waste radioactivity after about 104 to 106 years after the creation of the nuclear waste.[57] From 1945 to 1994, an estimated 160 TBq (about 250 kg) of technetium-99 was released into the environment during atmospheric nuclear tests.[57][59] The amount of technetium-99 from nuclear reactors released into the environment up to 1986 is on the order of 1000 TBq (about 1600 kg), primarily by nuclear fuel reprocessing; most of this was discharged into the sea. Reprocessing methods have reduced emissions since then, but as of 2005 the primary release of technetium-99 into the environment is by the Sellafield plant, which released an estimated 550 TBq (about 900 kg) from 1995–1999 into the Irish Sea.[58] From 2000 onwards the amount has been limited by regulation to 90 TBq (about 140 kg) per year.[60] Discharge of technetium into the sea resulted in contamination of some seafood with minuscule quantities of this element. For example, European lobster and fish from west Cumbria contain about 1 Bq/kg of technetium.[61][62][note 4]

Fission product for commercial use

The metastable isotope technetium-99m is continuously produced as a fission product from the fission of uranium or plutonium in nuclear reactors:

Because used fuel is allowed to stand for several years before reprocessing, all molybdenum-99 and technetium-99m is decayed by the time that the fission products are separated from the major actinides in conventional nuclear reprocessing. The liquid left after plutonium–uranium extraction (PUREX) contains a high concentration of technetium as TcO
4
but almost all of this is technetium-99, not technetium-99m.[63]

The vast majority of the technetium-99m used in medical work is produced by irradiating dedicated highly enriched uranium targets in a reactor, extracting molybdenum-99 from the targets in reprocessing facilities,[30] and recovering at the diagnostic center the technetium-99m produced upon decay of molybdenum-99.[64][65] Molybdenum-99 in the form of molybdate MoO2−
4
is adsorbed onto acid alumina (Al
2
O
3
) in a shielded column chromatograph inside a technetium-99m generator ("technetium cow", also occasionally called a "molybdenum cow"). Molybdenum-99 has a half-life of 67 hours, so short-lived technetium-99m (half-life: 6 hours), which results from its decay, is being constantly produced.[16] The soluble pertechnetate TcO
4
can then be chemically extracted by elution using a saline solution. A drawback of this process is that it requires targets containing uranium-235, which are subject to the security precautions of fissile materials.[66][67]

Almost two-thirds of the world's supply comes from two reactors; the National Research Universal Reactor at Chalk River Laboratories in Ontario, Canada, and the High Flux Reactor at Nuclear Research and Consultancy Group in Petten, Netherlands. All major reactors that produce technetium-99m were built in the 1960s and are close to the end of life. The two new Canadian Multipurpose Applied Physics Lattice Experiment reactors planned and built to produce 200% of the demand of technetium-99m relieved all other producers from building their own reactors. With the cancellation of the already tested reactors in 2008, the future supply of technetium-99m became problematic.[68]

The Chalk River reactor was shut down for maintenance in August 2009, and reopened in August 2010. The Petten reactor had a 6-month scheduled maintenance shutdown on Friday, February 19, 2010, and reopened September 2010.[69] With millions of procedures relying on technetium-99m every year, the low supply has left a gap, leaving some practitioners to revert to techniques not used for 20 years. Somewhat allaying this issue is an announcement from the Polish Maria research reactor that they have developed a technique to isolate technetium.[70]

Waste disposal

The long half-life of technetium-99 and its potential to form anionic species creates a major concern for long-term disposal of radioactive waste. Many of the processes designed to remove fission products in reprocessing plants aim at cationic species such as caesium (e.g., caesium-137) and strontium (e.g., strontium-90). Hence the pertechnetate escapes through those processes. Current disposal options favor burial in continental, geologically stable rock. The primary danger with such practice is the likelihood that the waste will contact water, which could leach radioactive contamination into the environment. The anionic pertechnetate and iodide tend not to adsorb into the surfaces of minerals, and are likely to be washed away. By comparison plutonium, uranium, and caesium tend to bind to soil particles. Technetium could be immobilized by some environments, such as microbial activity in lake bottom sediments,[71] and the environmental chemistry of technetium is an area of active research.[72]

An alternative disposal method, transmutation, has been demonstrated at CERN for technetium-99. In this process, the technetium (technetium-99 as a metal target) is bombarded with neutrons to form the short-lived technetium-100 (half-life = 16 seconds) which decays by beta decay to ruthenium-100. If recovery of usable ruthenium is a goal, an extremely pure technetium target is needed; if small traces of the minor actinides such as americium and curium are present in the target, they are likely to undergo fission and form more fission products which increase the radioactivity of the irradiated target. The formation of ruthenium-106 (half-life 374 days) from the 'fresh fission' is likely to increase the activity of the final ruthenium metal, which will then require a longer cooling time after irradiation before the ruthenium can be used.[73]

The actual separation of technetium-99 from spent nuclear fuel is a long process. During fuel reprocessing, it comes out as a component of the highly radioactive waste liquid. After sitting for several years, the radioactivity reduces to a level where extraction of the long-lived isotopes, including technetium-99, becomes feasible. A series of chemical processes yields technetium-99 metal of high purity.[74]

Neutron activation

Molybdenum-99, which decays to form technetium-99m, can be formed by the neutron activation of molybdenum-98.[75] When needed, other technetium isotopes are not produced in significant quantities by fission, but are manufactured by neutron irradiation of parent isotopes (for example, technetium-97 can be made by neutron irradiation of ruthenium-96).[76]

Particle accelerators

The feasibility of technetium-99m production with the 22-MeV-proton bombardment of a molybdenum-100 target in medical cyclotrons following the reaction 100Mo(p,2n)99mTc was demonstrated in 1971.[77] The recent shortages of medical technetium-99m reignited the interest in its production by proton bombardment of isotopically-enriched (>99.5%) molybdenum-100 targets.[78][79] Other techniques are being investigated for obtaining molybdenum-99 from molybdenum-100 via (n,2n) or (γ,n) reactions in particle accelerators.[80][81][82]

Applications

Nuclear medicine and biology

Technetium-99m ("m" indicates that this is a metastable nuclear isomer) is used in radioactive isotope medical tests. For example Technetium-99m is a radioactive tracer that medical imaging equipment tracks in the human body.[16][78] It is well suited to the role because it emits readily detectable 140 keV gamma rays, and its half-life is 6.01 hours (meaning that about 94% of it decays to technetium-99 in 24 hours).[22] The chemistry of technetium allows it to be bound to a variety of biochemical compounds, each of which determines how it is metabolized and deposited in the body, and this single isotope can be used for a multitude of diagnostic tests. More than 50 common radiopharmaceuticals are based on technetium-99m for imaging and functional studies of the brain, heart muscle, thyroid, lungs, liver, gall bladder, kidneys, skeleton, blood, and tumors.[83]

The longer-lived isotope, technetium-95m with a half-life of 61 days, is used as a radioactive tracer to study the movement of technetium in the environment and in plant and animal systems.[84]

Industrial and chemical

Technetium-99 decays almost entirely by beta decay, emitting beta particles with consistent low energies and no accompanying gamma rays. Moreover, its long half-life means that this emission decreases very slowly with time. It can also be extracted to a high chemical and isotopic purity from radioactive waste. For these reasons, it is a National Institute of Standards and Technology (NIST) standard beta emitter, and is used for equipment calibration.[85] Technetium-99 has also been proposed for optoelectronic devices and nanoscale nuclear batteries.[86]

Like rhenium and palladium, technetium can serve as a catalyst. In processes such as the dehydrogenation of isopropyl alcohol, it is a far more effective catalyst than either rhenium or palladium. However, its radioactivity is a major problem in safe catalytic applications.[87]

When steel is immersed in water, adding a small concentration (55 ppm) of potassium pertechnetate(VII) to the water protects the steel from corrosion, even if the temperature is raised to 250 °C (523 K).[88] For this reason, pertechnetate has been used as an anodic corrosion inhibitor for steel, although technetium's radioactivity poses problems that limit this application to self-contained systems.[89] While (for example) CrO2−
4
can also inhibit corrosion, it requires a concentration ten times as high. In one experiment, a specimen of carbon steel was kept in an aqueous solution of pertechnetate for 20 years and was still uncorroded.[88] The mechanism by which pertechnetate prevents corrosion is not well understood, but seems to involve the reversible formation of a thin surface layer (passivation). One theory holds that the pertechnetate reacts with the steel surface to form a layer of technetium dioxide which prevents further corrosion; the same effect explains how iron powder can be used to remove pertechnetate from water. (Activated carbon can also be used for the same purpose.) The effect disappears rapidly if the concentration of pertechnetate falls below the minimum concentration or if too high a concentration of other ions is added.[90]

As noted, the radioactive nature of technetium (3 MBq/L at the concentrations required) makes this corrosion protection impractical in almost all situations. Nevertheless, corrosion protection by pertechnetate ions was proposed (but never adopted) for use in boiling water reactors.[90]

Precautions

Technetium plays no natural biological role and is not normally found in the human body.[20] Technetium is produced in quantity by nuclear fission, and spreads more readily than many radionuclides. It appears to have low chemical toxicity. For example, no significant change in blood formula, body and organ weights, and food consumption could be detected for rats which ingested up to 15 µg of technetium-99 per gram of food for several weeks.[91] The radiological toxicity of technetium (per unit of mass) is a function of compound, type of radiation for the isotope in question, and the isotope's half-life.[92]

All isotopes of technetium must be handled carefully. The most common isotope, technetium-99, is a weak beta emitter; such radiation is stopped by the walls of laboratory glassware. The primary hazard when working with technetium is inhalation of dust; such radioactive contamination in the lungs can pose a significant cancer risk. For most work, careful handling in a fume hood is sufficient, and a glove box is not needed.[93]

Notes

  1. ^ In 1998 John T. Armstrong of the National Institute of Standards and Technology ran "computer simulations" of the 1925 experiments and obtained results quite close to those reported by the Noddack team. "Using first-principles X-ray-emission spectral-generation algorithms developed at NIST, I simulated the X-ray spectra that would be expected for Van Assche's initial estimates of the Noddacks' residue compositions. The first results were surprisingly close to their published spectrum! Over the next couple of years, we refined our reconstruction of their analytical methods and performed more sophisticated simulations. The agreement between simulated and reported spectra improved further. Our calculation of the amount of element 43 required to produce their spectrum is quite similar to the direct measurements of natural technetium abundance in uranium ore published in 1999 by Dave Curtis and colleagues at Los Alamos. We can find no other plausible explanation for the Noddacks' data than that they did indeed detect fission "masurium."
    Armstrong, J. T. (2003). "Technetium". Chemical & Engineering News. 81 (36): 110. doi:10.1021/cen-v081n036.p110. 
  2. ^ Irregular crystals and trace impurities raise this transition temperature to 11.2 K for 99.9% pure technetium powder.(Schwochau 2000, p. 96)
  3. ^ As of 2005, technetium-99 in the form of ammonium pertechnetate is available to holders of an Oak Ridge National Laboratory permit:Hammond, C. R. (2004). "The Elements". Handbook of Chemistry and Physics (81st ed.). CRC press. ISBN 0-8493-0485-7. 
  4. ^ The anaerobic, spore-forming bacteria in the Clostridium genus are able to reduce Tc(VII) to Tc(IV). Clostridia bacteria play a role in reducing iron, manganese, and uranium, thereby affecting these elements' solubility in soil and sediments. Their ability to reduce technetium may determine a large part of mobility of technetium in industrial wastes and other subsurface environments. Francis, A. J.; Dodge, C. J.; Meinken, G. E. (2002). "Biotransformation of pertechnetate by Clostridia". Radiochimica Acta. 90 (9–11): 791–797. doi:10.1524/ract.2002.90.9-11_2002.791. 
  1. ^ a b "Technetium: technetium(III) iodide compound data". OpenMOPAC.net. Retrieved 2007-12-10. 
  2. ^ Cverna, Fran (2002). "Ch. 2 Thermal Expansion". ASM Ready Reference: Thermal properties of metals (PDF). ASM International. ISBN 978-0-87170-768-0. 
  3. ^ Weast, Robert (1984). CRC, Handbook of Chemistry and Physics. Boca Raton, Florida: Chemical Rubber Company Publishing. pp. E110. ISBN 0-8493-0464-4. 
  4. ^ Jonge; Pauwels, E. K. (1996). "Technetium, the missing element". European Journal of Nuclear Medicine. 23 (3): 336–44. PMID 8599967. doi:10.1007/BF00837634. 
  5. ^ a b Holden, N. E. "History of the Origin of the Chemical Elements and Their Discoverers". Brookhaven National Laboratory. Retrieved 2009-05-05. 
  6. ^ Yoshihara, H. K. (2004). "Discovery of a new element 'nipponium': re-evaluation of pioneering works of Masataka Ogawa and his son Eijiro Ogawa". Spectrochimica Acta Part B. 59 (8): 1305–1310. Bibcode:2004AcSpe..59.1305Y. doi:10.1016/j.sab.2003.12.027. 
  7. ^ a b van der Krogt, P. "Elentymolgy and Elements Multidict, "Technetium"". Retrieved 2009-05-05. 
  8. ^ Emsley 2001, p. 423
  9. ^ Armstrong, J. T. (2003). "Technetium". Chemical & Engineering News. Chemical & Engineering News. 81 (36): 110. doi:10.1021/cen-v081n036.p110. Retrieved 2009-11-11. 
  10. ^ Nies, K. A. (2001). "Ida Tacke and the warfare behind the discovery of fission". Retrieved 2009-05-05. 
  11. ^ Weeks, M. E. (1933). "The discovery of the elements. XX. Recently discovered elements". Journal of Chemical Education. 10 (3): 161–170. Bibcode:1933JChEd..10..161W. doi:10.1021/ed010p161. 
  12. ^ Zingales, R. (2005). "From Masurium to Trinacrium: The Troubled Story of Element 43". Journal of Chemical Education. 82 (2): 221–227. Bibcode:2005JChEd..82..221Z. doi:10.1021/ed082p221. 
  13. ^ Heiserman 1992, p. 164
  14. ^ Segrè, Emilio (1993). A Mind Always in Motion: the Autobiography of Emilio Segrè. Berkeley, California: University of California Press. pp. 115–118. ISBN 0520076273. 
  15. ^ a b Perrier, C.; Segrè, E. (1947). "Technetium: The Element of Atomic Number 43". Nature. 159 (4027): 24. Bibcode:1947Natur.159...24P. PMID 20279068. doi:10.1038/159024a0. 
  16. ^ a b c d e Emsley, J. (2001). Nature's Building Blocks: An A-Z Guide to the Elements. New York: Oxford University Press. pp. 422–425. ISBN 0-19-850340-7. 
  17. ^ "Chapter 1.2: Early Days at the Berkeley Radiation Laboratory". The transuranium people: The inside story. University of California, Berkeley & Lawrence Berkeley National Laboratory. 2000. p. 15. ISBN 1-86094-087-0. 
  18. ^ Merrill, P. W. (1952). "Technetium in the stars". Science. 115 (2992): 479–89 [484]. Bibcode:1952Sci...115..479.. doi:10.1126/science.115.2992.479. 
  19. ^ a b c d Schwochau 2000, pp. 7–9
  20. ^ a b c d Hammond, C. R. (2004). "The Elements". Handbook of Chemistry and Physics (81st ed.). CRC press. ISBN 0-8493-0485-7. 
  21. ^ Lide, David R. (2004–2005). "Line Spectra of the Elements". The CRC Handbook. CRC press. pp. 10–70 (1672). ISBN 978-0-8493-0595-5. 
  22. ^ a b c d Rimshaw, S. J. (1968). Hampel, C. A., ed. The Encyclopedia of the Chemical Elements. New York: Reinhold Book Corporation. pp. 689–693. 
  23. ^ Schwochau, K. Technetium: Chemistry and Radiopharmaceutical Applications; Wiley-VCH:Weinheim, Germany, 2000.
  24. ^ Autler, S. H. (1968). "Technetium as a Material for AC Superconductivity Applications" (PDF). Proceedings of the 1968 Summer Study on Superconducting Devices and Accelerators. Retrieved 2009-05-05. 
  25. ^ Greenwood 1997, p. 1044
  26. ^ a b c Husted, R. (2003-12-15). "Technetium". Periodic Table of the Elements. Los Alamos National Laboratory. Retrieved 2009-10-11. 
  27. ^ Garraway, John (1984). "The technetium-catalysed oxidation of hydrazine by nitric acid". Journal of the Less Common Metals. 97: 191–203. doi:10.1016/0022-5088(84)90023-7. 
  28. ^ Garraway, J. (1985). "Coextraction of pertechnetate and zirconium by tri-n-butyl phosphate". Journal of the Less Common Metals. 106 (1): 183–192. doi:10.1016/0022-5088(85)90379-0. 
  29. ^ Schwochau 2000, pp. 127–136
  30. ^ a b Moore, P. W. (April 1984). "Technetium-99 in generator systems" (PDF). Journal of Nuclear Medicine. 25 (4): 499–502. PMID 6100549. Retrieved 2012-05-11. 
  31. ^ Krebs, B. (1969). "Technetium(VII)-oxid: Ein Übergangsmetalloxid mit Molekülstruktur im festen Zustand (Technetium(VII) Oxide, a Transition Metal Oxide with a Molecular Structure in the Solid State)". Angewandte Chemie. 81 (9): 328–329. doi:10.1002/ange.19690810905. 
  32. ^ Schwochau 2000, p. 127
  33. ^ Herrell, A. Y.; Busey, R. H.; Gayer, K. H. (1977). Technetium(VII) Oxide, in Inorganic Syntheses. XVII. pp. 155–158. ISBN 0-07-044327-0. 
  34. ^ Poineau F; Weck PF; German K; Maruk A; Kirakosyan G; Lukens W; Rego DB; et al. (2010). "Speciation of heptavalent technetium in sulfuric acid: structural and spectroscopic studies" (PDF). Dalton Transactions. 39 (37): 8616–8619. PMID 20730190. doi:10.1039/C0DT00695E. 
  35. ^ Schwochau 2000, p. 108
  36. ^ Schwochau 2000, pp. 112–113
  37. ^ Gibson, John K. (1993). "High-Temperature Oxide and Hydroxide Vapor Species of Technetium". Radiochimica Acta. 60 (2–3). doi:10.1524/ract.1993.60.23.121. 
  38. ^ Schwochau 2000, p. 146
  39. ^ Johnstone, E. V. (2014). "Binary Technetium Halides". 
  40. ^ a b c d Poineau, Frederic; Johnstone, Erik V.; Czerwinski, Kenneth R.; Sattelberger, Alfred P. (2014). "Recent Advances in Technetium Halide Chemistry". Accounts of Chemical Research. 47 (2): 624. PMID 24393028. doi:10.1021/ar400225b. 
  41. ^ Poineau, Frederic; Johnstone, Erik V.; Weck, Philippe F.; Kim, Eunja; Forster, Paul M.; Scott, Brian L.; Sattelberger, Alfred P.; Czerwinski, Kenneth R. (2010). "Synthesis and Structure of Technetium Trichloride". Journal of the American Chemical Society. 132 (45): 15864. PMID 20977207. doi:10.1021/ja105730e. 
  42. ^ German, K. E.; Kryutchkov, S. V. (2002). "Polynuclear Technetium Halide Clusters". Russian Journal of Inorganic Chemistry. 47 (4): 578–583. 
  43. ^ Bartholomä, Mark D.; Louie, Anika S.; Valliant, John F.; Zubieta, Jon (2010). "Technetium and Gallium Derived Radiopharmaceuticals: Comparing and Contrasting the Chemistry of Two Important Radiometals for the Molecular Imaging Era". Chemical Reviews. 110 (5): 2903. PMID 20415476. doi:10.1021/cr1000755. 
  44. ^ a b c Alberto, Roger (2010). "Organometallic Radiopharmaceuticals". Medicinal Organometallic Chemistry. Topics in Organometallic Chemistry. 32. p. 219. ISBN 978-3-642-13184-4. doi:10.1007/978-3-642-13185-1_9. 
  45. ^ Hileman, J. C.; Huggins, D. K.; Kaesz, H. D. (1961). "Technetium carbonyl". Journal of the American Chemical Society. 83 (13): 2953–2954. doi:10.1021/ja01474a038. 
  46. ^ Bailey, M. F.; Dahl, Lawrence F. (1965). "The Crystal Structure of Ditechnetium Decacarbonyl". Inorganic Chemistry. 4 (8): 1140–1145. doi:10.1021/ic50030a011. 
  47. ^ Wallach, D. (1962). "Unit cell and space group of technetium carbonyl, Tc2(CO)10". Acta Crystallographica. 15 (10): 1058. doi:10.1107/S0365110X62002789. 
  48. ^ Schwochau 2000, pp. 286, 328
  49. ^ Clayton, D. D. (1983). Principles of stellar evolution and nucleosynthesis: with a new preface. University of Chicago Press. p. 547. ISBN 0-226-10953-4. 
  50. ^ a b c d NNDC contributors (2008). Sonzogni, A. A., ed. "Chart of Nuclides". New York: National Nuclear Data Center, Brookhaven National Laboratory. Retrieved 2009-11-11. 
  51. ^ a b c d Holden, N. E. (2006). Lide. D. R., ed. Handbook of Chemistry and Physics (87th ed.). Boca Raton, Florida: CRC Press, Taylor & Francis Group. pp. 11–88–11–89. ISBN 0-8493-0487-3. 
  52. ^ Lide, David R., ed. (2004–2005). "Table of the isotopes". The CRC Handbook of Chemistry and Physics. CRC press. 
  53. ^ Dixon, P.; Curtis, David B.; Musgrave, John; Roensch, Fred; Roach, Jeff; Rokop, Don (1997). "Analysis of Naturally Produced Technetium and Plutonium in Geologic Materials". Analytical Chemistry. 69 (9): 1692–9. PMID 21639292. doi:10.1021/ac961159q. 
  54. ^ Curtis, D.; Fabryka-Martin, June; Dixon, Paul; Cramer, Jan (1999). "Nature's uncommon elements: plutonium and technetium". Geochimica et Cosmochimica Acta. 63 (2): 275. Bibcode:1999GeCoA..63..275C. doi:10.1016/S0016-7037(98)00282-8. 
  55. ^ Moore, C. E. (1951). "Technetium in the Sun". Science. New York, N.Y. 114 (2951): 59–61. Bibcode:1951Sci...114...59M. PMID 17782983. doi:10.1126/science.114.2951.59. 
  56. ^ Schwochau 2000, pp. 374–404
  57. ^ a b c Yoshihara, K. (1996). "Technetium in the Environment". In K. Yoshihara; T. Omori. Topics in Current Chemistry: Technetium and Rhenium. 176. Berlin Heidelberg: Springer-Verlag. pp. 17–35. ISBN 978-3-540-59469-7. doi:10.1007/3-540-59469-8_2. 
  58. ^ a b Garcia-Leon, M. (2005). "99Tc in the Environment: Sources, Distribution and Methods" (PDF). Journal of Nuclear and Radiochemical Sciences. 6 (3): 253–259. 
  59. ^ Desmet, G.; Myttenaere, C. (1986). Technetium in the environment. Springer. p. 69. ISBN 0-85334-421-3. 
  60. ^ Tagami, K. (2003). "Technetium-99 Behaviour in the Terrestrial Environment — Field Observations and Radiotracer Experiments". Journal of Nuclear and Radiochemical Sciences. 4: A1–A8. doi:10.14494/jnrs2000.4.a1. 
  61. ^ Szefer, P.; Nriagu, J. O. (2006). Mineral components in foods. CRC Press. p. 403. ISBN 0-8493-2234-0. 
  62. ^ Harrison, J. D.; Phipps, A. (2001). "Gut transfer and doses from environmental technetium". J. Radiol. Prot. 21 (1): 9–11. Bibcode:2001JRP....21....9H. PMID 11281541. doi:10.1088/0952-4746/21/1/004. 
  63. ^ Schwochau 2000, p. 39
  64. ^ US 3799883, Hirofumi Arino, "Silver coated charcoal step", issued March 26, 1974, assigned to Union Carbide Corporation 
  65. ^ Committee on Medical Isotope Production Without Highly Enriched Uranium (2009). Medical Isotope Production Without Highly Enriched Uranium. National Academies Press. p. vii. ISBN 0-309-13040-9. 
  66. ^ Lützenkirchen, K.-R. "Nuclear forensics sleuths trace the origin of trafficked material". Los Alamos National Laboratory. Archived from the original on 2013-02-16. Retrieved 2009-11-11. 
  67. ^ Snelgrove, J. L.; Hofman, G. L. (1995). "Development and Processing of LEU Targets for Mo-99 Production" (PDF). ANL.gov, Presented at the 1995 International Meeting on Reduced Enrichment for Research and Test Reactors, September 18–21, 1994, Paris, France. Retrieved 2009-05-05. 
  68. ^ Thomas, Gregory S.; Maddahi, Jamshid (2010). "The technetium shortage". Journal of Nuclear Cardiology. 17 (6): 993–8. PMID 20717761. doi:10.1007/s12350-010-9281-8. 
  69. ^ Shaw, Gina (October 2010). "Medical Isotope Shortage Nearing End—For Now". Clinical Oncology News. Retrieved 2010-11-02. 
  70. ^ Wals, M. L. (February 16, 2010). "New Source Of an Isotope In Medicine Is Found". New York Times. 
  71. ^ German, Konstantin E.; Firsova, E. V.; Peretrukhin, V. F.; Khizhnyak, T. V.; Simonoff, M. (2003). "Bioaccumulation of Tc, Pu, and Np on Bottom Sediments in Two Types of Freshwater Lakes of the Moscow Oblast". Radiochemistry. 45 (6): 250–6. doi:10.1023/A:1026008108860. 
  72. ^ Shaw, G. (2007). Radioactivity in the terrestrial environment. Elsevier. p. 147. ISBN 0-08-043872-5. 
  73. ^ Altomare, P; Bernardi (1979). Alternative disposal concepts for high-level and transuranic radioactive waste disposal. US Environmental Protection Agency. 
  74. ^ Schwochau 2000, pp. 87–96
  75. ^ "Manual for reactor produced radioisotopes" (PDF). IAEA. January 2003. Retrieved 2009-08-27. 
  76. ^ Kelly, J. J. (1980). Effluent and environmental radiation surveillance: a symposium. ASTM International. p. 91. 
  77. ^ Beaver, J. E.; Hupf, H.B. (November 1971). "Production of 99mTc on a Medical Cyclotron: a Feasibility Study" (PDF). Journal of Nuclear Medicine. 12 (11): 739–41. PMID 5113635. 
  78. ^ a b Laurence Knight (30 May 2015). "The element that can make bones glow". BBC. Retrieved 30 May 2015. 
  79. ^ Guérin B; Tremblay S; Rodrigue S; Rousseau JA; Dumulon-Perreault V; Lecomte R; van Lier JE; et al. (2010). "Cyclotron production of 99mTc: an approach to the medical isotope crisis" (PDF). Journal of Nuclear Medicine. 51 (4): 13N–6N. PMID 20351346. 
  80. ^ Scholten, Bernhard; Lambrecht, Richard M.; Cogneau, Michel; Vera Ruiz, Hernan; Qaim, Syed M. (25 May 1999). "Excitation functions for the cyclotron production of 99mTc and 99Mo". Applied Radiation and Isotopes. 51 (1): 69–80. doi:10.1016/S0969-8043(98)00153-5. 
  81. ^ Takács, S.; Szűcs, Z.; Tárkányi, F.; Hermanne, A.; Sonck, M. (1 January 2003). "Evaluation of proton induced reactions on 100Mo: New cross sections for production of 99mTc and 99Mo". Journal of Radioanalytical and Nuclear Chemistry. 257 (1): 195–201. doi:10.1023/A:1024790520036. 
  82. ^ Celler, A.; Hou, X.; Bénard, F.; Ruth, T. (2011). "Theoretical modeling of yields for proton-induced reactions on natural and enriched molybdenum targets". Physics in Medicine and Biology. 56 (17): 5469–5484. Bibcode:2011PMB....56.5469C. PMID 21813960. doi:10.1088/0031-9155/56/17/002. 
  83. ^ Schwochau 2000, p. 414
  84. ^ Schwochau 2000, pp. 12–27
  85. ^ Schwochau 2000, p. 87
  86. ^ "University Research Program in Robotics REPORT" (PDF). University of Florida. 2006-11-30. Retrieved 2007-10-12. 
  87. ^ Schwochau 2000, pp. 87–90
  88. ^ a b Emsley 2001, p. 425
  89. ^ "Ch. 14 Separation Techniques". EPA: 402-b-04-001b-14-final (PDF). US Environmental Protection Agency. July 2004. Archived from the original on 2014-03-08. Retrieved 2008-08-04. 
  90. ^ a b Schwochau 2000, p. 91
  91. ^ Desmet, G.; Myttenaere, C.; Commission of the European Communities. Radiation Protection Programme, France. Service d'études et de recherches sur l'environnement, United States. Dept. of Energy. Office of Health and Environmental Research (1986). Technetium in the environment. Springer. pp. 392–395. ISBN 0-85334-421-3. 
  92. ^ Schwochau 2000, pp. 371–381
  93. ^ Schwochau 2000, p. 40

Bibliography

Further reading



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Periodic Table Of Elements

element,system,atom,molecule,metal,halogen,noble gas,chemical,chemistry