powered by CADENAS

Social Share

Anhydrous (10059 views - Material Database)

A substance is anhydrous if it contains no water, for example, salts lacking their water of crystallization. The way of achieving the anhydrous form differs from one substance to another.
Go to Article

Anhydrous

Anhydrous

A substance is anhydrous if it contains no water, for example, salts lacking their water of crystallization.[1] The way of achieving the anhydrous form differs from one substance to another.

Solvents

In many cases, the presence of water can prevent a reaction from happening, or it can cause undesirable products to form. To prevent this, anhydrous solvents must be used when performing certain reactions. Examples of reactions requiring the use of anhydrous solvents are the Grignard reaction and the Wurtz reaction.

Solvents are commonly rendered anhydrous by boiling them in the presence of a hygroscopic substance; metallic sodium is one of the most common metals used. Other methods include the addition of molecular sieves or alkali bases such as potassium hydroxide or barium oxide. Column solvent purification devices (generally referred to as Grubb's columns) recently became available, reducing the hazards (water reactive substances, heat) from the classical dehydrating methods.[2][3]

Gases

Several substances that exist as gases at standard conditions of temperature and pressure are commonly used as concentrated aqueous solutions. To clarify that it is the gaseous form that is being referred to, the term anhydrous is prefixed to the name of the substance:

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

Datenbank,rohs,reach,Compliancy,Verzeichnis,Liste,Information,Substanz,Material,Restriktion,Datenblatt,Spezifikation