powered by CADENAS

Social Share

Amazon

Floating hinge (5250 views - Maschinenbau)

A floating hinge is a hinge that, while able to behave as a normal hinge, enables one of the objects to move away from the other - hence float. In effect the hinge allows for two parallel axes of rotation, one for each object joined by the hinge, and each axis can be moved relative to the position of the other.
Go to Article

Explanation by Hotspot Model

Youtube


    

Floating hinge

Floating hinge

A floating hinge is a hinge that, while able to behave as a normal hinge, enables one of the objects to move away from the other - hence float. In effect the hinge allows for two parallel axes of rotation, one for each object joined by the hinge, and each axis can be moved relative to the position of the other.[1]

Uses

Floating hinges are used in flatbed scanners designed to scan thick objects such as books. A sheet of paper is placed on the glass, and the cover is lowered over it; the glass, the paper, and the sheet are very close together. If a thick book is placed on the glass an ordinary hinge would leave the cover at an angle to the glass. A floating hinge raises the hinged edge of the cover to the level of the book, so that the cover remains parallel to the glass, but raised above it.[2]

Floating hinges are also used in two-plate electric cooking grills, as they allow for even heating of both sides of a thick piece of food without crushing it.[3]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Maschinenbau

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD