Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Slip joint pliers are pliers whose pivot point or fulcrum can be moved to increase the size range of their jaws. Most slip joint pliers use a mechanism that allows sliding the pivot point into one of several positions when the pliers are fully opened.
There are many different varieties of slip joint pliers, including straight slip joint pliers, tongue-and-groove pliers and lineman's pliers.
Straight slip joint pliers are configured similarly to common or lineman's pliers in that their jaws are in line with their handles. One side of the pliers usually has two holes that are connected by a slot for the pivot. The pivot is fastened to the other side and shaped such that it can slide through the slot when the pliers are fully opened.
Tongue-and-groove pliers have their jaws offset from their handles and have several positions at which the lower jaw can be positioned.
This tool article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
tooling,tool,drill,cam,manufacturing