powered by CADENAS

Social Share

Amazon

Clam (3921 views - Animals)

Clam is a common name for several kinds of bivalve molluscs. The word is often applied only to those that are edible and live as infauna, spending most of their lives halfway buried in the sand of the seafloor. Clams have two shells of equal size connected by two adductor muscles and have a powerful burrowing foot. Clams in the culinary sense do not live attached to a substrate (whereas oysters and mussels do) and do not live near the bottom (whereas scallops do). In culinary usage, clams are commonly eaten marine bivalves, as in clam digging and the resulting soup, clam chowder. Many edible clams such as palourde clams are oval or triangular; however, razor clams have an elongated parallel-sided shell, suggesting an old-fashioned straight razor.Some clams have life cycles of only one year, while at least one may be over 500 years old. All clams have two calcareous shells or valves joined near a hinge with a flexible ligament, and all are filter feeders.
Go to Article

Explanation by Hotspot Model

Youtube


    

Clam

Clam

Clam is a common name for several kinds of bivalve molluscs. The word is often applied only to those that are edible and live as infauna, spending most of their lives halfway buried in the sand of the seafloor. Clams have two shells of equal size connected by two adductor muscles and have a powerful burrowing foot.[1] Clams in the culinary sense do not live attached to a substrate (whereas oysters and mussels do) and do not live near the bottom (whereas scallops do). In culinary usage, clams are commonly eaten marine bivalves, as in clam digging and the resulting soup, clam chowder. Many edible clams such as palourde clams are oval or triangular;[2] however, razor clams have an elongated parallel-sided shell, suggesting an old-fashioned straight razor.[3]

Some clams have life cycles of only one year, while at least one may be over 500 years old.[4] All clams have two calcareous shells or valves joined near a hinge with a flexible ligament, and all are filter feeders.

Anatomy

A clam's shell consists of two (usually equal) valves, which are connected by a hinge joint and a ligament that can be external or internal. The ligament provides tension to bring the valves apart, while one or two adductor muscles can contract to close the valves. Clams also have kidneys, a heart, a mouth, a stomach, a nervous system and a butt. Many have a siphon.

As food

North America

In culinary use, within the eastern coast of the United States and large swathes of the Maritimes of Canada, the term "clam" most often refers to the hard clam Mercenaria mercenaria. It may also refer to a few other common edible species, such as the soft-shell clam, Mya arenaria and the ocean quahog, Arctica islandica. Another species commercially exploited on the Atlantic Coast of the United States is the surf clam Spisula solidissima. Scallops are also used for food nationwide, but not cockles: they are more difficult to get than in Europe because of their habit of being farther out in the tide than European species on the West Coast, and on the East Coast they are often found in salt marshes and mudflats where mosquitoes are abundant.[5][6] Up and down the coast of the Eastern U.S., the bamboo clam, ensis directus, is prized by Americans for making clam strips although because of its nature of burrowing into the sand very close to the beach, it cannot be harvested by mechanical means without damaging the beaches.[7] The bamboo clam is also notorious for having a very sharp edge of its shell, and when harvested by hand must be handled with great care.

On the U.S. West Coast, there are several species that have been consumed for thousands of years, evidenced by middens full of clamshells near the shore and their consumption by nations including the Chumash of California, the Nisqually of Washington State and the Tsawwassen of British Columbia.[8][9][10][11] The butter clam, Saxidomus gigantea,[12] the Pacific razor clam, Siliqua patula, [13] gaper clams Tresus capax,[14] the geoduck clam, Panopea generosa [15] and the Pismo clam, Tivela stultorum [16] are all eaten as delicacies.

Clams can be eaten raw, steamed, boiled, baked or fried. They can also be made into clam chowder, clams casino, Clam cakes, stuffies, or they can be cooked using hot rocks and seaweed in a New England clam bake. On the West Coast, they are an ingredient in making cioppino and local variants of ceviche[17]

Japan

In Japan, clams are often an ingredient of mixed seafood dishes. They can also be made into hot pot, miso soup or Tsukudani. The more commonly used varieties of clams in Japanese cooking are the Shijimi (Corbicula japonica), the Asari (Venerupis philippinarum) and the Hamaguri (Meretrix lusoria).[citation needed]

Italy

In Italy, clams are often an ingredient of mixed seafood dishes or are eaten together with pasta. The more commonly used varieties of clams in Italian cooking are the Vongola (Venerupis decussata), the Cozza (Mytilus galloprovincialis) and the Tellina (Donax trunculus). Though Dattero di mare (Lithophaga lithophaga) was once eaten, overfishing drove it to the verge of extinction (it takes 15 to 35 years to reach adult size and could only be harvested by smashing the calcarean rocks that form its habitat) and the Italian government has declared it an endangered species since 1998 and its harvest and sale are forbidden.[citation needed]

India

Clams are eaten more in the coastal regions of India, especially in the Konkan, Kerala, Bengal and coastal regions of Karnataka regions.[citation needed]

In Kerala clams are used to make curries and fried with coconut. In Malabar region it is known as "elambakka" and in middle kerala it is known as "kakka". Clam curry made with coconut is a dish from Malabar especially in the Thalassery region. On the south western coast of India, also known as the Konkan region of Maharashtra, clams are used in curries and side dishes, like Tisaryachi Ekshipi, which is clams with one shell on. Beary Muslim households in the Mangalore region prepare a main dish with clams called Kowldo Pinde. In Udupi and Mangalore regions it is famously called as "marvai" in local tulu language. It is used to prepare many delicious dishes like marvai sukka, marvai gassi, and marvai pundi.[citation needed]

Trinidad and Tobago

Local fishermen sell them in rural markets.[citation needed]

Religion

In Judaism, clams are considered non-kosher (treif); But in Islam, clams are considered Halal along with all other shellfish, which lack a fish's fins and scales.[18]

As currency

Some species of clams, particularly Mercenaria mercenaria, were in the past used by the Algonquians of Eastern North America to manufacture wampum, a type of sacred jewelry; and to make shell money.[19]

Species

Edible:

Not usually considered edible:

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Animals

3D,data,libary,model,catalog,rendering,skull,bone,animal,reptile,bird,insect,mammal,class,classification,order,family,species,genus