This message means that a licensefile is in use which date of maintenance expired.
Solutions:
1. Usage of valid licensefile and make sure this is the only/ unique licensefile used (press F1-button in PARTsolutions
for documentation).
if you do not have a valid licensefile:
2. Contact your local PARTsolutionsdealer to receive actual licensefile.
3. Contact your local PARTsolutionsdealer for renewal of maintenancecontract.
1. Please use the form which can download with the following link:
Hardware exchange
2. For licensing the Host-ID (MAC address) of the old and the new computer is required.
-> The Host-ID can be selected in the license manager PARTadmin.
3. Get further help regarding licensing by clicking F1 within PARTsolutions
In the Category menu mark the item License administration -> Clients.
Select the Licenses index page.
Select a license product top right.
-> Now detailed license information is displayed under License key and Host ID/Role.
Check, whether all received licenses are listed.
If the license file „*.cnsldb“ is not listed or you have received a new license file, which you want to add to the list, then do the following:
--> Now the file is listed in the license administration.
Mark the License file in the dialog area top right.
--> The individual License keys with Expiration date and Status are listed.
Check, whether the Host ID of the license (downright) is according to one of the Host ID displayed above (see Fig. „Licenses“).
(Exception: Some products (e.g. free catalogs) have so-called zero-licenses '0000 0000 0000'). Here the hostid doesn't have to be according)
In order for the license to be effective for the respective module (PARTdataManager, etc.), the Status has to be OK (green).
In order to finish the procedure, click on the Save changes button! (If not already happened during the license installation).
Call up software and support information
After double-click on a license file / license product (*.cnsldb) the Software information dialog box appears.
In the Customer information dialog area you can find your Customer number. Stating the number helps the support better help you.
Under Dealer information you can find the relevant dealer with Support e-mail and support phone number.
As of V9.03 catalogs without valid license are displayed in their own category under PARTadmin -> PARTsolutions -> Catalog update-> Online -> Catalogs, no valid license.
Get further help regarding licensing by clicking F1 within PARTsolutions