Follow the steps listed below to define the characteristic of the part:
Make sure that you are in the dialog area 3D CAD CATALOGS and search for the required part.
At directory level select product groups as long as a concrete assembly or concrete single part has been specified and choose an assembly or a single part.
Define the characteristic of the part, by clicking into the option field of the desired row.
-> A default view of the selected model which may differ from the selected characteristic, is displayed under CAD model preview.
Note
If you want to view an exact replication of the characteristic, under Actions click on Generate preview.
Switch to the variable view by clicking on the part description.
The variable view shows all important data of a specific characteristic in a compact form.