Mozilla Firefox is a leading net browser, just like UC Browser, Google Chrome, Internet Explorer, etc. In fact, it is the second-highest used browsers in the allover world. It is famous in customers because of its advance aspects and feature's. But with a lot of compliments, it is also having some problem, and the most common issue is Firefox freeze's, or Mozilla Firefox keep's freezing. But, there is nothing to worry about because this search engine is also a part of technology running on the internet, and we all know that technology can be stuck sometime's; however, there is always a solution. Therefore, here we will discuss the remedies of Mozilla keeps freezing.
How to deal with the problem Firefox Keeps Freezing?
Disable the automatic update
If automatic update is enabled in your devices, it may lead to a lot of hurdles and confusions in the smooth running of the browser. Follow the step to enable this setting:
Open Mozilla icon
Click on the tools option available on the topmost section
Select “Add-ons” from the given tools
Now it will redirect you to the “options.”
Click on Advanced tab given on the topmost right side of the screen
Click on the update tab
Now “check for the update; however, let me choose whether to install them.”
Now click on ok for final submission.
Remove extra Add-ons from Firefox.
An incompatible and outdated model of Add-ons may freeze Firefox. So we have to disable on those add-ons:
Open Mozilla Icon
When browser loads successfully, click on Tool's given on top
Then select Add ons from the provided tools
Now you’ll come to the Tools Manager screen
Click on Extensions, moving forward click on Next.
Then scroll down and click on Remove / Disable Add-ons from there. But while removing, make sure to remove which is not relevant for you in any vital program.
Restart or refresh your browser before using it.
Mozilla Firefox is a leading net browser, just like UC Browser, Google Chrome, Internet Explorer, etc. In fact, it is the second-highest used browsers in the allover world. It is famous in customers because of its advance aspects and feature's. But with a lot of compliments, it is also having some problem, and the most common issue is Firefox freeze's, or Mozilla Firefox keep's freezing. But, there is nothing to worry about because this search engine is also a part of technology running on the internet, and we all know that technology can be stuck sometime's; however, there is always a solution. Therefore, here we will discuss the remedies of Mozilla keeps freezing.
How to deal with the problem Firefox Keeps Freezing?
Disable the automatic update
If automatic update is enabled in your devices, it may lead to a lot of hurdles and confusions in the smooth running of the browser. Follow the step to enable this setting:
Open Mozilla icon
Click on the tools option available on the topmost section
Select “Add-ons” from the given tools
Now it will redirect you to the “options.”
Click on Advanced tab given on the topmost right side of the screen
Click on the update tab
Now “check for the update; however, let me choose whether to install them.”
Now click on ok for final submission.
Remove extra Add-ons from Firefox.
An incompatible and outdated model of Add-ons may freeze Firefox. So we have to disable on those add-ons:
Open Mozilla Icon
When browser loads successfully, click on Tool's given on top
Then select Add ons from the provided tools
Now you’ll come to the Tools Manager screen
Click on Extensions, moving forward click on Next.
Then scroll down and click on Remove / Disable Add-ons from there. But while removing, make sure to remove which is not relevant for you in any vital program.
Restart or refresh your browser before using it.
When Windows senses that something could cause real harm, it stops everything, ie screen freezing occurs which results in the appearance of the blue screen. Blue screens are usually generated by dilemmas with the computer's hardware or issues with their hardware driver software. repeater gsm
When Windows senses that something could cause real harm, it stops everything, ie screen freezing occurs which results in the appearance of the blue screen. Blue screens are usually generated by dilemmas with the computer's hardware or issues with their hardware driver software. repeater gsm
A most effective way to resolve this issue is to update your browser or reinstall it. But there are some alternatives you should try them. I recommend you to try the best 5 web browsers for Windows and macOS.
A most effective way to resolve this issue is to update your browser or reinstall it. But there are some alternatives you should try them. I recommend you to try the best 5 web browsers for Windows and macOS.