powered by CADENAS

BIMcatalogs.net beim open BIM FORUM 2019, Luzern, Schweiz » Discussions


When should you replace your exterior door?

  • February 25, 2023

    When should you replace your exterior door?

  • February 25, 2023

    Like windows, doors can also cause unwanted and uncomfortable drafts. Air can enter through cracks around your door, creating discomfort in your home and putting stress on your home's heating, ventilation, and air conditioning system. Installing a new front door will eliminate unpleasant drafts and increase the energy efficiency of your home.


    A trick to check for drafts is to light a candle or lighter and run it across the door frame. If the flame is moving towards you, this indicates an air leak.

  • February 25, 2023

    Is your door difficult to open and close? Once you close it, is it hard to block it? In the summer, your door may be more difficult to open because the wood can expand and swell with moisture, making it difficult to work. The front door should not be difficult to operate, it should be easy to open and close. If you find it difficult to open and close your door, it might be time to consider a replacement. You can contact TH Windows and Doors Oakville to resolve this issue. These Oakville exterior doors https://oakvillewindowsanddoors.ca/exterior-doors-oakville/ are made from quality materials. They offer different options for doors and at reasonable prices.

  • May 12, 2023

    Are you tired of your old, boring exterior door?

  • May 12, 2023

    Do you want to give your home a fresh new look? Well, the answer is simple - replace your exterior door! With TH Windows and Doors Whitby, you can rest assured that your home renovations will be a success. But when should you replace your exterior door? If you see any signs of wear and tear, such as cracks, warping or rotting, it's time to replace it! Not only will a new  front door whitby enhance the appearance of your home, but it will also improve its security and energy efficiency. So why wait? Upgrade your home with TH Windows and Doors Whitby today!

  • May 24, 2023

    There are several indicators that can help you determine when it's time to replace your exterior door. If your current exterior door does not provide adequate security, interior designers in lahore essential to consider a replacement. Outdated or compromised doors can be easier targets for burglars. Upgrading to a more secure door, such as one with a solid core or reinforced glass, can enhance your home's security.

  • Jan 7

    Drafts can be persistent adversaries in our quest for a cozy home. While a new door might seem like the obvious fix, it's essential to delve deeper into the root causes of drafts.

  • Jan 7

    Often, gaps and leaks around windows, walls, and even the roof can contribute significantly to the infiltration of cold air. Overlooking these areas during an energy audit could render a door replacement ineffective in addressing the draft dilemma.

  • Jan 7

    Energy efficiency is a complex puzzle, and focusing solely on the entrance doors neglects other crucial components of your home's thermal envelope.

  • Jan 7

    If you decide to replace the doors in your home, then you should think about renovating at least the hallway of your home. After all, replacing doors is only the first step.