With their components on 3DfindIT.com and PARTcommunity powered by CADENAS, the 3D CAD product catalogs of component manufacturers are now really taking off: In the month of June 2020, engineers, architects and purchasers downloaded 56,353,866 CAD & BIM models from renowned manufacturers worldwide for the first time, providing them with a steadily increasing number of valuable sales leads.
The innovative search engine 3DfindIT.com from CADENAS was launched in June 2019. Conventional search engines focus specifically on delivering search results that are as suitable for everyday use as possible. However, these are often unsuitable or irrelevant for engineering and architecture. Using 3DfindIT.com, manufacturers and their components can be integrated directly into the CAD & BIM designs of engineers and architects as well as into the respective parts lists. These are then finally procured by the purchasing department. Studies show that in 87% of cases, downloading engineering data later leads to a real purchase of the product.
Comments