powered by CADENAS

News

Photo

Social Share

News Entry

(EN) Updated BIMcatalogs.net plugin powered by CADENAS: BIM objects directly available in Revit 2021, ARCHICAD 23 & Allplan 2020

  • Access to manufacturer verified BIM objects with LOD directly within CAD system

    CADENAS is releasing a new version of its popular BIMcatalogs.net plugin: From now on, architects and planners can use it to access original, manufacturer-verified BIM and CAD models directly in Autodesk Revit 2021, GRAPHISOFT ARCHICAD 23 and Nemetschek Allplan 2020 and integrate them quickly and easily into their designs. In addition, the new plugin version allows users to set filters for supplier countries for selected catalogs for the first time. This ensures from the very first moment that the desired product can be delivered to its destination.

    Direct access to BIM objects with LOD in the BIM planning system

    The BIMcatalogs.net Plugin is seamlessly integrated with the CAD systems Revit, ARCHICAD, ALLPLAN, SketchUp and Tekla. It enables architects and planners to easily search, select and configure the available BIM objects directly in their familiar software environment. Much of the BIM data supports different levels of development (LOD), allowing users to easily switch between different LODs during the design process.

    Always current manufacturer data

    The BIMcatalogs.net plugin has a consistent link to the original manufacturer data, which means that the inserted products are always up to date. When product information is changed, these changes are automatically applied to existing designs.

    For example, Autodesk Revit users benefit from the BIMcatalogs.net plugin:

    The BIMcatalogs.net plugin is available for free download at: www.bimcatalogs.net/cadapp

Comments

0 comments