powered by CADENAS

News

Photo

Social Share

News Entry

(EN) This is how it works: Provide augmented reality (AR) in PARTcloud.net and 3D CAD models with various environments

  • If you wish to make your 3D model appealing, you should try out the environment function

    Augmented Reality (AR) is understood as computer-assisted extension of the perception of reality. Frequently, images or videos are supplemented with additional information or virtual objects by means of overlaying or superimposing. So if you want to expand your CAD model with additional information, there are various options to choose from in the sharing community PARTcloud.net, e.g. various images and optical design variations:

    Under "Environment" there are some environment images available in which the 3D model can be added. As an alternative, only the floor of the model can be designed. The users here can choose from diverse images.

    And this is the way it works:

    • First, users have to login at PARTcloud.net or create an account free of charge in order to enjoy all the advantages of the Sharing Community. If you are already registered for the 3D CAD models download portal PARTcommunity, this is also valid for PARTcloud.net.
    • The components are uploaded and the information as well as details filled in so that the 3D CAD model can be found more easily by other users.
    PARTcloud.net
    • After uploading, the 3D CAD model appears in your own portfolio.
    PARTcloud.net
    • The users now activate the environment function by moving the cursor to the lower bar and clicking the last button.
    PARTcloud.net
    • A new window appears, where the environments can be selected. Here are different environments available to the users, such as city silhouette and floor variants such as parquet. Both options can be selected at the same time.
    PARTcloud.net
    • At the end, the users obtain their 3D model with the selected background. Now they can put the model in the scene accordingly per screenshot or in the PARTcloud.net app or add the image at social networks.
    PARTcloud.net

    By the way: Find out how to provide your model with additional information here.

    Try it out right away: Share and receive 3D CAD models

    Whoever is a part of the large Sharing Community will benefit both from the enormous selection of user-generated CAD models and from the platform itself, in order to upload his own models and to make them available to other users.

    It's best to go to www.partcloud.net right away and join the Sharing Community

    PARTcloud.net available also as an app

    Upload your own 3D CAD models as well as browse around in the product range or search for specific parts with diverse searching functions on the go as well with the PARTcloud.net app for Android, iOS and Windows 10.

    PARTcloud.net for Android

    PARTcloud.net for Android
    You can find further information and the free download on Google Play.

    PARTcloud.net on Google Play

    PARTcloud.net for iOS

    PARTcloud.net for iOS
    You can find further information and the free download on iTunes.

    PARTcloud.net on iTunes

    PARTcloud.net for Windows 10

    PARTcloud.net for Windows 10
    You can find further information and the free download on Microsoft Store.

    PARTcloud.net on Microsoft Store

    3D CAD models download portal PARTcommunity

    If you are in search of manufacturer-certified CAD catalogs, you are at the right place with 3D CAD models download portal PARTcommunity. Look around right away at: www.partcommunity.com

    CADENAS - The Innovation Company

    CADENAS - The Innovation CompanyTo achieve excellence, copying is not enough – CADENAS - The Innovation Company

Comments

0 comments