powered by CADENAS

News

Photo

Social Share

News Entry

(EN) Don’t let yourself be fooled!

  • Even when the human eye fails, CADENAS’ Geometric Similarity Search GEOsearch won’t let you down

    At first sight, many things seem to be different than what they actually are. This is most evident in the case of so-called optical illusions. Here various areas of eyesight can be affected: Illusions of depth and color, geometric illusions or illusions of motion etc.

    This video is a good example for an optical illusion. It shows the best illusion of the year by Kohichi Sugihara from the “Illusion of the Year Contest 2016“:

    The human eye can hardly recognize why one and the same object appears to be sections of circles while in the other view sections of rectangles. If you could hold the objects in your hands you would immediately figure out the trick: The cylinders don’t have straight edges, they are corrugated - the top of the sides are wave patterns, two sides dip up and two sides dip down. The combination of the object’s structure and the perspective lead to an illusion for the eyes, since they try to compensate for the wave pattern.

    Find similar components with the Geometric Similarity Search GEOsearch

    Also when designing, one always needs a good eye and different parts. When looking for a suitable 3D CAD model, it is usually not possible to touch it, so you need other tools to figure out differences. Good if tools are available that cannot be fooled, like CADENAS’ Geometric Similarity Search GEOsearch from the Strategic Parts Management PARTsolutions. This search feature looks for parts by means of the respective CAD geometry and compares them to each other. Starting with a reference part or a roughly sketched 3D model, all existing CAD components of the parts database can be searched just like with a search engine.

    Check it out now!

    Not only in the Strategic Parts Management PARTsolutions and the 3D CAD model download portal PARTcommunity offers Geometric Similarity Search: Also with CADENAS’ exchange platform for parts, PARTcloud.net, you now have the option to find CAD models by means of similar geometric data. Upload your part now and get right below similar models! Check it out now!

    Also with CADENAS’ exchange platform for parts, PARTcloud.net, you now have the option to find CAD models by means of similar geometric data.

    You can find the cylinders Ambicylinder 4 Position Rectangle and Ambicylinder 4 Position Circle for download on PARTcloud.net.

    Upload your own 3D CAD models and try out which “twins“ PARTcloud.net can find for you. Curious? Then just click here.