powered by CADENAS

News

Author

Eddie Choi

Recent Entries

  • (EN) Mencom Introduces New lock designs to secure MIN Series Connections for Harsh Manufacturing Environments at IMTS – Booth #E-415

    Mencom Introduces New lock designs to secure MIN Series Connections for Harsh Manufacturing Environments at IMTS – Booth #E-4152 in the East Building Connection failures can be caused by various reasons, such as excess temperature, excess current or voltage, mechanical shock, stress and impac...
  • (EN) Mencom Corporation Introduces New Front Mount M12 Circular Receptacles with Front Lock Nut for Harsh Manufacturing Environments

    Mencom Corporation Introduces New Front Mount M12 Circular Receptacles with Front Lock Nut for Harsh Manufacturing Environments at IMTS – Booth #E-4152 in the East Building   Mencom is pleased to announce new front locking nut technology for our M12 connectors. These front mount recepta...
  • (EN) Mencom introduces new tool-free cable entry system

    Mencom Corporation Introduces New System for the Insertion and Sealing of Cables for Harsh Manufacturing Environments at IMTS – Booth #E-4152 in the East Building  KADP cable entry system offers a simpler and faster assembly for inserting and sealing cables for enclosures, machines and j...
  • (EN) Mencom Announces New MIL-Spec Industrial 5015 Equivalent Connectors

    The MIL-Spec 5015 series was originally designed for severe aeronautical and tactical service applications. Due to the rugged and versatile design, these connectors are widely used in a range of commercial and industrial applications, such as factory automation, robotics, instrumentation, medical eq...
  • (EN) Mencom Electrical Connectors for Industrial Automation

    Automation is a key part of almost all manufacturing today. Some of the main benefits of Industrial Automation are: Reduced Costs What once took one or more people to do, can now be accomplished with one robot, which contributes to significant reduction in material handling, orientation time, par...
  • (EN) The Benefits of Panel Interface Connector Private Labeling

    Mencom offers private labeling for Panel Interface Connectors also known as programming ports or program ports. For high volume OEM customers, Mencom, the brand leader in Panel Interface Connectors, can customize the label with clients’ company information and place onto the front of their Pan...
  • (EN) Mencom Announces the Fully Responsive Website Launch

    Mencom Corporation, the leading US based manufacturer of industrial electrical connectors since 1987 and the North American master distributor of ILME rectangular connectors, is proud to announce the launch of their fully responsive version of their website. This mobile friendly website offers quick...
  • (EN) Mencom Waterproof Connectors for Harsh Environments

    Mencom Corp. will be featuring its waterproof connectors for harsh manufacturing environments at PackExpo 2015 – Booth S-6378 in the Lower South Hall in the Las Vegas Convention Center.   There are as many terms used to describe waterproof connectors as there are reasons for needin...
  • (EN) Mencom Announces New Plastic Port Adapters

    NEW Plastic Port Adapters now available Mencom now offers their classic port adapters in a low profile black plastic shell with a M25 mounting thread.  They are rated IP65, which means they provide total protection against dust and jets of water from all directions.  These new plastic por...
  • (EN) Cable Jacket Performance Guide

    The choice of cable jacket will depend on many factors such as extreme temperature, a variety of liquid and chemicals and physically abusive environment. The infographic shows a summary of the properties of the most commonly used materials, PVC, PUR and TPE, to help facilitate a better decision on t...
  • (EN) M12 & 1/2-20″ Connectors Keyway Chart

    Circular M12 and ½-20″ cordsets and receptacles are available in a variety of pin configurations and wire color codes. In addition to a variety of pin out and color code differences, each of these connectors also has distinct keyways. Below is a chart displaying these keyways.
  • (EN) Mencom Field Wireable Connectors Size Comparison

    Mencom Field Wireable Connectors offer plug-and-play connectivity for electrical wiring to make installation easier in various applications. They are available in M8, M12 A-Code (Micro-DC & DeviceNet), M12 B-Code (Euro-AC & Profibus), M12 D-Code (Ethernet & Profinet), 1/2"-20 C-Code&n...
  • (EN) Solenoid Valve Connectors

    In engineering, the term solenoid refers to a variety of transducer devices that convert energy into linear motion. The term is also often used to refer to a solenoid valve, which is an integrated device containing an electromechanical solenoid which actuates either a pneumatic or hydraulic valve, o...
  • (EN) Mencom Gets UL Listing

    We are pleased to announce Mencom’s products have been certified for compliance with both Canadian and U.S. safety requirements by Underwriters Laboratories (UL), and the UL Listed mark now appears on our end products. UL is a non-profit organization that has developed more than 1,000 safety s...
  • (EN) Meet Top quality & Low cost Thermoplastic Insulating Enclosures

    When it comes to heavy duty rectangular connectors, Mencom Corp. is the North American master distributor of ILME, an international market leader offering exceptional quality with competitive pricing. Continuing with the same tradition of quality and value, Mencom Corp. is pleased to introduce ILME ...
  • (EN) NEW T35 Expandable Din Rail Terminal Modules

    Mencom’s new expandable T35 series of Din Rail modules allow you the convenience of mounting a wide variety of connectors to your DIN rail. Also known as “break-out boards” these modules allow the end user to take a pre-molded connection, like a ribbon cable or D-Sub, and easily br...
  • (EN) Fast & reliable solutions for connectivity between sensor & control panel

    Mencom's quick disconnect sensor connectors and cabling offers fast and reliable solutions for the connectivity between the sensors and the control panel. Our sensor cables are over-molded with a variety of outer jacket material with or without shielding to provide the next line of defense for ...
  • (EN) Introducing the ILME CSH series of inserts “SQUICH” Connections without tools!

    Cabling time : 50% quicker than the screw-type connection and 20% quicker than the conventional spring-type connection, and CSH connector inserts can be mated with the corresponding inserts of series CNE, CSE, CCE, CTE, CTSE, CN, CT and CSS. The CSH series “SQUICH” offers the following ...
  • (EN) Why Do You Need Panel Interface Connectors?

    A panel interface connector also known as programming ports is a device that typically mounts to the outside of a control panel housing a PLC, computer, or other type of programmable device. Once in place, the PIC, which houses convenient pass through connections, allows quick, easy, ...
  • (EN) ILME kits and pre-wired receptacles from Mencom

    Mencom Corporation is now offering ILME kits consisting of the main components needed to make your connection, and pre-wired ILME receptacles.  Both solutions are designed to help drastically reduce labor time and costs associated with product installation. ILME connectors are known for the...