powered by CADENAS

News

Photo

Social Share

News Entry

(EN) https://www.mencom.com/news/case-study-el-pomar

  • About El Pomar

    El Pomar is a Colombian dairy company founded in 1953. They wanted to improve electrical safety at the factory.

    The Goal

    In order to achieve electrical safety, they were looking for solutions that could provide employees with a safer working environment and better protect electrical equipment at the production site while reducing the risk of downtime.

    The Challenges

    The most critical components in their equipment are the milk sterilizer, the enzyme dosing system, and powdered milk packaging machines. Unfortunately, they were all built with different installations and wiring by different manufacturers. They also operate independently in three different low-quality electrical cabinets. While the machines can be operated safely by employees without an electrical license, these complex connections from different applications should be streamlined.

    The Solution

    CGS Optimize (www.cgsoptimize.com), a Mencom distributor in Colombia, suggested building one high-quality electrical cabinet to operate all machines in, instead of the three current cabinets. The key components of this cabinet, which were integrated to achieve the goal, were Mencom’s Low-profile Panel Interface Connectors and USB Port Adapters.

    The Outcome

    Mencom Panel Interface connectors and USB Port adapters allowed the PLC to operate without opening the cabinet while protecting the operators and securing the connection. As a result, the solutions performed by CGS Optimize could significantly reduce the risks of electrical accidents and help save PLC programming time. All these solutions were achieved without interfering with the factory production and El Pomar could successfully centralize the equipment operation into the one cabinet for the first time, standardizing all programming and operating routines.   

     

    Spanish Version

    Acerca de El Pomar

    El Pomar es una empresa lactea Colombiana fundada en 1953, que buscaba mejorar la seguridad eléctrica de su planta.

    El Objetivo

    Para lograr mayor seguridad eléctrica, necesitaba soluciones que también le ofrezca a los empleados condiciones laborales mas seguras y una mayor protección eléctrica a los equipos en la planta, reduciendo riesgos de paradas no planificado (downtime).

    Los Desafios

    Los equipos más importantes de la planta son esterilizadores de leche, dosificadores de enzima y empacadora de bolsa de leche. Desafortunadamente, estos equipos son de distintas marcas, con cableados y configuraciones diferentes, y son operados desde distintos gabinetes con escasa seguridad. Aunque estos equipos pueden ser operados con cierta seguridad por los empleados sin una licencia eléctrica, estas complejas conexiones de diferentes aplicaciones deberían ser estandarizadas.

    La Solución

    CGS Optimize (www.cgsoptimize.com), distribuidor de Mencom en Colombia, le sugirió a El Pomar la construcción de un gabinete de alta calidad para centralizar los controles desde ahí, reemplazando los tres actuales. Los componentes clave de este nuevo gabinete son el Panel de interface de bajo perfil y un Panel de Puerto USB, ambos de Mencom.

    El Resultado

    El Panel Interface y el Panel de Puerto USB de Mencom les permitió operar el PLC y generar reportes sin necesidad de abrir el gabinete, protegiendo operadores y conexiones internas. Como resultado, se disminuyeron riesgos de accidentes eléctricos y ahorraron tiempo de operación y programación sin detener los procesos productivos. A su vez, se lograron operar todos los equipos desde un solo gabinete, estandarizando configuraciones y facilitando el operado del mismo.