Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
1. Quality from AMF
There are very good reasons why a discriminating user should choose the best quality screwdriving tools:
> rigorous quality control ensures uniform standards
> seen as a whole, more economical, because the unproductive time spent while tools are issued is reduced to the essential minimum
> in sizes up to ca. 6 A/F, the torque that can be applied by hand may be higher than the test torque that is specified in the relevant standard, with the resualt that:
the wrench deforms, but only breaks under very unfavourable conditions, a modest, but valuable contribution is made to safety in the workplace;
> the true value of quality tools can only be seen in real, practical use
2. Material
Highly alloyed chrome-vnadium steel
> tested steel sections in verifiably uniform quality from trusted suppliers ensure low wear for a long working-life.
3. Manufacture
> end faces machined
> end face up to 10 mm jaw opening chamfered process-sure
> inspection by sampling at all stages of production
4. Execution
Hardness to DIN standards
> the values of minimum torque specified for tightening screws up to grade 12.9 are achieved or exceeded.
5. Surface finish
> blued (Version C)
> nickel-plated (Version D)