Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to check the integrity of a part click on the button Test part . Integrity has to be ensured to avoid error messages in QA check and finally a faultless export to the different CAD systems is ensured.
If there are problems when executing the function this is immediately documented in the 3D view.
In the following you can see some examples for construction errors:
A definition for "non-manifold" related to praxis is: You could not machine the shape out of a single block.
In the 3D History the affected element is marked by a red cross .
The dialog box Notifications shows the error.
In the dialog box QA check the error message Non manifold is also displayed.
Error message "The result is more than one solid"
The shape cannot be machined out of a single block.
In the 3D History a red cross is displayed at affected elements.
The dialog box Notifications shows an error. "The objects are not connected".
In the dialog box QA check The error message "The objects are not connected" is also displayed".