Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The general settings indicated below concern the blocks [STLIMPORT], [PREVIEWIMPORT] and [VIEWIMPORT] equally.
Reference to the imported files
The
reference can either be given directly with the key "PATH" or,
in the section "CSV_ImageImport", you refer to the file
filelist.txt
,
which contains the path specification.
Direct path specification in the configuration file
[STLIMPORT / PREVIEWIMPORT / VIEWIMPORT] PATH=\\someserver\bmpDir bzw. PATH1=\\someserver\bmpDir
If, in the configuration
file under $CADENAS/classimport.cfg
in the section "CSV_ImageImport" you refer to your own
definition file (filelist.txt
) and
the paths are specified there, the specification under "PATH"
and/or "PATH1" is not needed.
Example for import via "filelist.txt" file
If
you are using OnVariant, as well as OnClass, it is best to
apply two areas in the text file filelist.txt
as shown in
the image.
If no STL file is found, the default file is used.
DEFAULTFILE=C:/import/default.stl
Delete original files in the input directory after import
[STLIMPORT / PREVIEWIMPORT / VIEWIMPORT] delInput1=0/1
For value = '1' the original files in the input directory are deleted according to the batch.
Name assignment and/or convention
[STLIMPORT / PREVIEWIMPORT / VIEWIMPORT] NAMEINPUT1=%name%.bmp
Here the names of the files in the input directory are determined:
[STLIMPORT / PREVIEWIMPORT / VIEWIMPORT] NAMEPOOL1=%name%_view1.bmp
Here the file name in the pool directory ($CADENAS_DATA\pool\insertpool\23d-natives\nativepool\STLFILE\) is defined: