Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
(both conditions - right and left of .AND. - must be filled out) |
|
(one of the two conditions - right or left of .OR. - must be filled out) |
|
The following examples show key values:
(ERP_PDM_NUMBER.NE.'')
The expression is true, if the respective field of the column ERP_PDM_NUMBER is not equal empty.
((ERP_PDM_NUMBER.NE.'').AND.(ACTIVE_STATE.EQ.1))
The expression is true, if the respective field of the column ERP_PDM_NUMBER is not equal empty AND the respective field of the column ACTIVE_STATE has the value 1 (=Released).
(PRICE.LT.0.4)
The expression is true, if the respective field of the column PRICE has a value lower or equal than 0,4.
(REQUESTED_STATE.EQ.2)
The expression is true, if the respective field of the column REQUESTED_STATE has the value 2 (=Expired).
((ACTIVE_STATE.EQ.1).AND.(LOCATION1.NE.''))
The expression is true, if the respective field of the column ACTIVE_STATE has the value 1 (=Released) AND the respective field of the column LOCATION1 is not equal empty.
(CONTAINS(ERP_PDM_NUMBER,'AA').EQ..TRUE.)
The expression is true, if the respective field of the column ERP_PDM_NUMBER contains the substring 'AA'.
(CONTAINS(ERP_PDM_NUMBER,'AA').EQ..FALSE.)
The expression is true, if the respective field of the column ERP_PDM_NUMBER does NOT contain the substring 'AA'.