Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Roles and rights
are set via configuration file $CADENAS_SETUP/partwarehouse/accessrights.cfg
.
In order to be able to perform settings for catalog and subdirectories you need the internal IDs CatalogID and Identification.
Then under Show internal ids for attributes, classes and products activate the checkbox.
-> Now on the tabbed page Properties, you can see the fields CatalogID and Identification in addition. Exactly this additional information is needed in order to perform certain settings in the configuration file.
Block: The block declaration is a combination of role and catalog.
[<Rolle>.<Katalog>]
Objects (keys) for which access rights (values) can be defined:
Valid access rights (values) are: (single entry or multiple entries comma separated or all)
For example, you can set minimal rights (only read access) as default:
[default] catalogs=read attributes=read products=read classes=read
The "Admin" role gets full access to all catalogs.
[admin.*] catalogs=add,modify,delete,read,export attributes=add,modify,delete,read products=add,modify,delete,read classes=add,modify,delete,read
The command "Export to PARTsolutions" is only displayed if (on the server), in the key "catalogs" the value "export" is set.
All roles get access for a certain catalog.
[*.jLRR0DPBQdm3HerWv3Jwuw] catalogs=read attributes=read products=read
In addition to catalog also subdirectories can get specific access conditions.
subtree.izWhloO_R2yDcz_5oRKGqQ=add,modify,delete
[werk1.jLRR0DPBQdm3HerWv3Jwuw] attributes=add,modify,delete products=add,modify,delete
One certain role and all catalogs + specification only for products
[werk1.*] products=add,modify,delete
If there is only read access in the structure tree the "lock" icon is displayed.