The BHC SR-N4 is the world's largest non-military hovercraft. It carries 418 passengers and 60 cars.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RruxI1je
The Bagger 288 weighs 13,500 tons, spans 215 ft and is about 100 ft high.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrveU5vp
Liebherr T 282B is the largest, highest capacity haul truck in the world that could transport up to 400 tons.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrtgkJba
Krupp's Bagger 288 is the world's largest digging machine. It is also considered the world's largest vehicle.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrvHpi43
The Crawler Transporter is the second largest vehicle in the world. It costs only $14 million to produce.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2Rrucv4f7
Antonov An-225 is the largest and heaviest aircraft in the world.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RruJeY4n
The Crawler Transporter weighs close to 3,000 tonnes, and travels with a maximum speed of one mile per hour.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrupU5kV
The Russian Zubr class LCAC is the largest military hovercarft. It can transport three battle tanks, 140 fully equipped troops, or up to 130 tons of cargo.
Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrvA7w2U