Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A second Condition should make sure that the Length of the butterfly screw is oriented to the Thickness of the plate. The screw may never be shorter than the plate height + 4mm.
So in the dialog box Condition properties following expression has to be stated:
PLATE@H+4<=BUTTERFLYSCREW@L
For the procedure go in line with the approach described under Section 9.7.2.4.2, “Defining first condition ”.
-> Dialog area Configurator: The second condition (if) <Name of condition> (here "Length") shows up.
Under Assembly, select "plate". -> The corresponding table is displayed.
Now select the characteristic with Hight 6 mm for H, for example.
Under Assembly, click on "butterflyscrew". -> Corresponding table shows up.
-> Only butterfly screws with a length equal or greater than 10 mm are available for selection.
-> The conditions are fulfilled: