powered by CADENAS

Board Info

Board Options

Social Share

Board Details

(EN) Monster Machines

Impressive machines from all over the world
  • 0 likes
  • 3317 views
  • 23 pins

created April 29, 2013 in Technology

Board Content

  • 0 likes
  • 0 comments
  • 0 repins
To produce stunning images of our galaxy, your rinky-dink smartphone camera just isn’t going to cut it. No, to generate 9GP masterpieces, you’ll need to use the world’s largest infrared survey telescope outfitted with the world’s largest infrared camera.
  • 0 likes
  • 0 comments
  • 0 repins
The little orange digger and the man don't stand a chance against this white monster of a machine.
  • 0 likes
  • 0 comments
  • 0 repins
A colossal 28-wheel truck that will help build a major telescope array in the Chilean Andes The giant vehicle will heave antennas – each weighing 115 tonnes – up a mountainside to the site of the array, a plateau 5,000m above sea level. The antenna transporter is 10m wide, 20m long and 6m high. It weighs 130 tonnes and has as much power as two Formula 1 engines. The first of two vehicles has been put through its paces at the firm Scheuerle Fahrzeugfabrik near Stuttgart in Germany. The vehicles will have to haul their heavy cargo safely from the 2,900m-high Alma base camp, where the antennas are assembled, to the array site, which lies at 5,000m – about half the cruising altitude of a 747. Because of the low oxygen content of the air at 5,000m, vehicle operators will need to wear portable oxygen canisters. The backrests of the driver seats are shaped to allow the driver to wear his oxygen tank while driving.
  • 0 likes
  • 0 comments
  • 0 repins
The world’s largest wheel loader.
  • 0 likes
  • 0 comments
  • 0 repins
Monster Machines on Land Survey Job Site
  • 0 likes
  • 0 comments
  • 0 repins
Surface coal mining in area Kolubara, Serbia
  • 0 likes
  • 0 comments
  • 0 repins
The Bagger 288 can excavate about 240,000 tons of coal daily. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrvpN5MK
  • 0 likes
  • 0 comments
  • 0 repins
The Bagger 288 weighs 13,500 tons, spans 215 ft and is about 100 ft high. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrveU5vp
  • 0 likes
  • 0 comments
  • 0 repins
Krupp's Bagger 288 is the world's largest digging machine. It is also considered the world's largest vehicle. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrvHpi43
  • 0 likes
  • 0 comments
  • 0 repins
The Russian Zubr class LCAC is the largest military hovercarft. It can transport three battle tanks, 140 fully equipped troops, or up to 130 tons of cargo. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrvA7w2U
  • 0 likes
  • 0 comments
  • 0 repins
The BHC SR-N4 is the world's largest non-military hovercraft. It carries 418 passengers and 60 cars. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RruxI1je
  • 0 likes
  • 0 comments
  • 0 repins
The Crawler Transporter weighs close to 3,000 tonnes, and travels with a maximum speed of one mile per hour. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrupU5kV
  • 0 likes
  • 0 comments
  • 0 repins
The Crawler Transporter is the second largest vehicle in the world. It costs only $14 million to produce. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2Rrucv4f7
  • 0 likes
  • 0 comments
  • 0 repins
Antonov An-225 is the largest and heaviest aircraft in the world. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RruJeY4n
  • 0 likes
  • 0 comments
  • 0 repins
Liebherr T 282B is the largest, highest capacity haul truck in the world that could transport up to 400 tons. Read more: http://www.businessinsider.com/biggest-machines-2010-10?op=1#ixzz2RrtgkJba