Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Export Options are saved in the configuration
file exportdlls.cfg
.
In order to ensure a consistent workflow it may make sense to set default values.
(For single users
there is no need for adjustments, as their changes are saved under $CADENAS_USER/exportdll.cfg
and
will be available at the next call again.)
Note | |
---|---|
Normally
defaults are set under The Here, defaults have to be set under
|
In order to perform desired settings, best proceed as follows:
With a sample part, perform an export.
Open the
corresponding configuration file $CADENAS_USER/exportdlls.cfg
and copy the block [RecentFiles]
into the
same-named file under $CADENAS_SITESETUP
(or create
it), rename the block to [Settings]
and delete not
required keys, especially those with path statements.
[Settings] DWG2D_OPTPAGEDWGEXPORT_solidColor=VAL{"1"} DWG2D_OPTPAGEDWGEXPORT_thinColor=VAL{"3"} DWG2D_OPTPAGEDWGEXPORT_hiddenLinetype=VAL{"dashed"} DWF2D_OPTPAGEDWGEXPORT_insertPointX=VAL{90} DWF2D_OPTPAGEDWGEXPORT_insertPointY=VAL{20} EPS_OPTPAGEEPS_thinWeight=VAL{"0.3"} CATV4IUA2D_OPTPAGEVECTOR_grouped=VAL{-1} CATV4IUA2D_OPTPAGEMETA2DV2_Rebase=VAL{0} DWG3D_OPTPAGEMETA3DV2_draft2sweep=VAL{1} DXF3D_OPTPAGEMETA3DV2_splitpattern=VAL{1} BMP_OPTPAGEIMAGE_Width=VAL{100} BMP_OPTPAGEIMAGE_Height=VAL{100} ...
Settings from
$CADENAS_USER/exportdlls.cfg
and
$CADENAS_SITESETUP/exportdlls.cfg
are
merged. If conflicts occur the settings under $CADENAS_USER/exportdlls.cfg
win.