Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Do you want to display data from your ERP and/or PDM system such as article number, descriptions, release status, material, surface, storage information, prices, etc. in the PARTdataManager?
PARTdataManager: The columns "ERP number", "Description" and "Material" (in the figure) are just exemplarily for any information from third party systems.
Then these data have to be linked in the LinkDB with the corresponding standard and supplier parts of PARTsolutions catalogs.
ERP/PDM system are able to export article data in the form of a CSV file.
The module PARTdataCenter will automatically establish the link between the PARTsolutions characteristic attribute table and the corresponding CSV information. The number of datasets which can be linked by an automatic process depends on the quality of data. Using different filters, products which couldn't be uniquely assigned yet are filtered and so can be systematically processed. Furthermore the user interface enables a manual processing in addition.
For getting
started quickly use the provided exemplary CSV files. These only contain a
few lines (characteristics) by which all important can be explained. You can
find these files under "$CADENAS/training/partdatacenter/article_number_assignment/
".
Customer administration, ERP consultant
| ||||
[a] Generally: Specific parameters to determine the characteristic |
| ||||
[b] You can find an example on this under Section 3.1.6.2, “ Article Number Search with regular expression”. |
LinkDB connection must be possible. As an alternative, product assignments / link information can be saved in a CSV file in an intermediate step and later be imported into the LinkDB.
The PARTsolutions target catalog has to be installed (for the following examples mostly the Standards catalog).