powered by CADENAS

Manual

Manual

3.2.5. "Products" category

When selecting the Products category on the left side then the single products are listed on the right side.

[Note] Note

The products view contains ALL products of the catalog.

However, after the export back to PARTsolutions, only classified products are component of the catalog, in other words those products which are in the Structure category.

[Note] Note

If the products view is empty you have either to add products (see Section 3.2.5.2, “ Add Product ”) or the view type List is selected and you have to explicitly determine attributes for the view (see Section 3.2.5.1, “Display type Table | List | Tiles ”).

The following listing gives an overview on the single functions of the Products view. There you find links to detailed information, if available.

Buttons

Context menu commands