powered by CADENAS

Manual

Manual

3.1.11.4. Product view - Context menu commands

The following listing contains context menu commands needed for article assignment.

Context menu commands on linked project line

Context menu commands on linked project line

  • Change category to ... - > Valid / Invalid

    In the context menu of each product line you can find the context menu command Change category to ... -> Valid or Invalid. By default, the link is Invalid.

    If you mark an assignment suggestion explicitly as valid, the respective line is marked with a green bar.

    Markup with green bar

    Markup with green bar

    The markup can be used as filter when exporting into the LinkDB. There you have the option only to export lines which are marked as Valid. See Section 3.1.9, “LinkDB export (Directly or via CSV file)”.

  • Modify link: Characteristic attribute table with variables is displayed. Used to adjust variables of variants. On this see under Section 3.1.5.3, “Optional settings in the node "Line Finder NENN"”.

  • Open link: Open linked part in PARTdataManager.

  • Create comment ...: Select predefined comment which is displayed in the comment field then.

    • product group not available

    • product dimension/type not available

    • product description incomplete

  • Remove link: Removes the currently selected assignment

  • Remove not valid links from current product

  • Remove not valid links from catalog

  • Remove category in all catalogs: All assignments of all catalogs are removed

    Whenever a process is executed new links are created and the old ones are not deleted. With the help of this command you can make sure that you will always start on a "clean" state.

  • Remove category from catalog: Remove all assignments from the current catalog

    Whenever a process is executed new links are created and the old ones are not deleted. With the help of this command you can make sure that you will always start on a "clean" state.