powered by CADENAS

Manual

Manual

2.2.13.  Assign parts per geometrical search.

Based on any part of your catalog you can perform a geometric similarity search.

Therefor proceed as follows:

  1. Select the desired project in the index tree and load it.

    -> The Part view opens.

  2. Click on Assign parts per geometrical search. either in the toolbar or in the context menu.

    --> The same-named dialog opens.

    Here in the exemplarily fig. "Spezialschrauben" is activated and the "Move selection into class of the master part" command is used

    Here in the exemplarily fig. "Spezialschrauben" is activated and the "Move selection into class of the master part" command is used

    Stepwise do the following:

    1. Class (master part)

    Check whether the correct path is displayed.

    2. Selection of a variant

    Choose the desired characteristic in the list field under ERP number. This setting here is determining, NOT the selection in the table.

    Now the search part for the geometric search is uniquely defined.

    3. Directories

    In this dialog area you define the directories to be searched.

    The root directory of your native catalog is set by default.

    With the and button you can add/delete other directories.

    4. Search templates

    Choose the desired search template.

    [Note] Note

    In order that all templates work make sure that all fingerprints have been created. See Section 2.2.14, “ Update ... ”.

    5. Search

    - Define the maximum number of displayed search results.

    - Search results with lower degree of similarity (in %) are hidden.

  3. When all settings are made click on the Start search button.

    --> In the 6. Result dialog area all detected parts are listed.

  4. Assign parts

    1. Move selection into class of the master part:

      For all parts you want to move into the search project activate the checkbox. Click the respective button.

    2. Move master part into each class of the selection:

      For that projects whereto you want to move the master part activate the checkbox. Click the respective button.

  5. Close the dialog window with Cancel.