Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With the CADENAS Classimporter you can transfer classifications together with article master data to PARTsolutions.
Via PARTadmin category Index administration -> Geometry import the input files are prepared for the processing with the Classimporter.
The following steps explain the procedure. You can find a detailed documentation concerning Classimporter under Section 2.1, “ Classimporter ”.
If you want
to keep the converted stl-, or zjv files in the "import_temp"
directory, then under $CADENAS_USER/padmin.cfg
in
the "STLImportInput" section the "cleanup" key has
to be set on the value 0 (possibly you have to create the key).
Otherwise the directory is deleted after finished import.
The "import_temp" directory is found in the source directory.
The file
image.csv
references there:
"MATNR";"CLASSNAME";"STLFILE";"PREVIEWFILE" "";"4bar1";"C:/Program Files/SolidWorks Corp/SolidWorks/samples/HandsOn/addmotor/ import_temp/4bar1.zjv";""
With PARTadmin import the geometry files from the defined Source directory.
You can find a detailed description of the Import geometry data dialog box under Import von Geometrie-Dateien.
When all settings are made, then start the import with .
The following processes are executed:
-> The
files needed for the "Classimport" process (attrdata.csv,
attrdef.csv, erpdata.csv, image.csv, prjtable.csv, structure.csv,
structuredef.csv) are automatically written and saved under
$CADENAS_USER/PARTImporter
.
"ATTRIBUTE_NAME";"ATTRIBUTE_FL_VALUE";"ATTRIBUTE_FL_MAX_VALUE";"ATTRIBUTE_VALUE";... "CLASSNAME";"";"";"4bar1";"4bar1";"4bar1" "CLASSNAME";"";"";"part1";"part1";"part1" "CLASSNAME";"";"";"part2";"part2";"part2" "CLASSNAME";"";"";"part3";"part3";"part3" "CLASSNAME";"";"";"part4";"part4";"part4"
-> The
file classimport.cfg
is
automatically created in a way, that a number of settings required
for the Classimport process are already set.
The
path declaration in the [CSV_ClassStructure] section for example
is already adjusted correctly to $CADENAS_USER/PARTImporter
.
[CSV_ClassStructure] FILE=C:/Users/jflotho/AppData/Roaming/cadenas/partsolutions_v9/ PARTImporter/structure.csv etc.
The key "ADAPTFILENAMES" for STL, preview images and Wantfiles has been set to 0. Leave this setting.
[STLIMPORT] ADAPTFILENAMES=0 [PREVIEWIMPORT] ADAPTFILENAMES=0 [WANTFILEIMPORT] ADAPTFILENAMES=0
The catalog is created or updated (according to the setting).