Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Information on the different calling options of the dialog box Add new attribute can be found under Section 3.2.4, “"Attributes" category”.
To add a new attribute fill in the fields in the dialog box or select the desired option in the list fields.
When exporting to PARTsolutions the respective settings are performed.
Name: Enter the variable name (here exemplified "Info1").
The name appears in PARTdataManager, in the table as column name in bold font.
Description: Enter the variable description.
When clicking on the flag a list field opens where you can enter translations.
The description is displayed in PARTdataManager, in the table, below the variable name in the set $CADENAS_LANGUAGE.. Compare figure above.
Columns specified as Document are shown as green columns in PARTdataManager. A detailed description on this can be found under Section 3.2.4.1.1, “Document columns”.
Role: Details on this can be found under Section 8.5.2.2.2, “ Identification type ” in eCATALOGsolutions Manual.
Unit: If needed you can open the list field with click on .
Visibility -> Attribute visible: Concerns the visibility in PARTsolutions.
If the respective attribute had been hidden in PARTproject, here, the option is automatically set to "invisible" when importing, and vice versa when exporting the setting is used in PARTdataManager.
Both classes and attributes can be set as „visible“ or „invisible". Invisible classes are displayed with a transparent folder icon in PARTdataCenter as a note, which otherwise has no further effects.