powered by CADENAS

Manual

Manual

2.2.12.  Edit project in batch mode

Via Edit project in batch mode you can change the attribute values of a certain variable for all project rows in batch mode.

Therefor proceed as follows:

  1. Open the Part view (table) at the desired project.

  2. Click on Edit project in batch mode in the toolbar or in the context menu.

    --> The same-named dialog opens.

  3. All attributes of the selected project are listed.

    Mark the desired attribute row in the dialog window.

  4. Insert the desired value or value range into the Feature value field.

    (Under Edit dataset you can see the original attribute values.)

    [Note] Note

    Optionally you can set table restrictions. Then changes are only processed in all visible project rows.

  5. Confirm with Ok.

  6. Load the changed project and check the value range of the changed variable at different rows.

    The displayed values are correct

    The displayed values are correct