powered by CADENAS

Manual

Manual

2.1.5.5.2. Value range fields

Value range fields can also be show in PARTdataManager.

PARTdataManager - Part view

PARTdataManager - Part view

Value range fields can be defined as:

  • Lists

  • Areas

  • Both

In order for the value range field to be shown in color and work according to plan in the PARTdataManager, you must set the following:

  • Settings in attributedef.txt

    In the columns ATWITHLIST (value list) and ATWITHRANGE (value range) set an 'x' for the desired class name (CLASSNAME) and attribute name (ATTNAME), if you wish to have this function.

    ATWITHLIST and ATWITHRANGE

    ATWITHLIST and ATWITHRANGE

  • Settings in attributedata.txt

    List of values

    If a list of values is desired then apply the corresponding row several times.

    In the following figure matnr6 is applied three time with the attribute 'L' (under ATTRIBUTE_NAME). The displayed value is located under ATTRIBUTE_FL_VALUE, since we are talking about a floating number value; with a text the entry must occur under ATTRIBUTE_VALUE.

    Value range

    If a value range is desired, the enter the maximum value in the ATTRIBUTE_FL_MAX_VALUE column.

    Settings for value range and list of values

    Settings for value range and list of values

If you click on the value range field "L=100" in the PARTdataManager (see example), the window Enter value shows up.

In addition to an area selection of 100,000 to 200,000 the single values 250,000 and 300,000 show up as well.

Material number with List of values and Value range

Material number with List of values and Value range