powered by CADENAS

Manual

Manual

1.1.5.3. Optional settings in the node "Line Finder NENN"

  • Methods to analyze NENN

    • NENN text mapping analysis:

      Hits only when nearly 100% accordance in text and number is given

      With interchanged numbers there are no results.

  • NENN number mapping analysis:

    Only numbers are used for the analysis. The sequence of numbers doesn't matter primarily.

    If this option is selected, under Number mapping settings further options for specification are available. If the checkbox is cleared, the following options are not available.

    • Allow variants:

      If the option is deactivated, there is no further analysis for a not assignable product.

      Variant not recognized

      Variant not recognized

      If the option is activated, variants can often be recognized. They are marked with "Type = V' and the variant variable is displayed with its value.

      Variant recognized - However, assignment has still to be confirmed manually.

      Variant recognized - However, assignment has still to be confirmed manually.

      Open the context menu and click on Modify link.

      -> The project table is opened. The next fitting line is already automatically selected. Furthermore the variant variable is highlighted with green color.

      You just have to click Ok.

      -> Now the assignment is displayed with 100%.

    • User defined separators between attribute and value (Regular Expression):

      If you want to use several separators, use the pipe "|" as separator.

      Example:

      =|\s

      As separator "equal sign" OR "empty space" is specified.

      Example where the declaration of a separator makes sense.

      Example where the declaration of a separator makes sense.

      The sequence of the attribute-value pairs doesn't matter:

      "L=25, D=20" would have been found just as well.

    • User defined column positions:

      If several variable values are in one single column, you can use this function.

      In the column "Abmessung [Dimension]]" you can find the values for D and L.

      In the column "Abmessung [Dimension]]" you can find the values for D and L.

      Special case "empty input value"

      Example:

      Following input:

      20, 30, 46453456346

      Meaning: D=20, L = 30, Customer number=46453456346

      If the NENN algorithm detects, that the NENN may consist of 2 (D,L) or 3 (D,L,P) numbers, it attempts to match the third value "46453456346" to P, even it is not set explicitly in the column positions.

      However, in this case 46453456346 is not P, but the customer number.

      In this case you should not specify a variable as third input value. Then the NENN algorithm isn't used with 3 numbers, but with 2:

      D     First input value
      L     Second imput value
            Third input value

      The third input value is ignored and only D=20, L=30 are searched.