powered by CADENAS

Manual

Manual

1.3.6.6.1.  Show change history / Show history of products in subtree
[Note] Note

The history only concerns committed changes, not local ones which have been reverted by the Revert changes command.

The history can be used for research but also to restore a certain version with all changes up to the chosen point.

There are two commands for showing the history:

  • Show change history: All class changes are shown (name, description, class features)

  • Show history of products in subtree: All events of that products are shown which are assigned to a class in the subtree.

Example:

  1. In the context menu of a class, call the command Show change history.

    -> The dialog box Show History opens.

  2. Select an event. For this event you can call the context menu command Show Diff to current version.[9]

  3. Once an event is selected and you have clicked on OK, the status of the selected version is restored.

  4. Afterwards commit the changes.

Also see Section 1.3.6.6.3, “Revert committed changes”.



[9] only at "Show history", not at "Show history of products in subtree"