Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If on the side of PARTsolutions the physical properties are set in the CNS classification, then these are also transferred to the CAD system during the export.
In PARTdataManager the attributes of the CNS classification are displayed under index tree, context menu of a part, menu item Part information.
In the following is explained how Solid Edge acts in different scenarios.
If a material has been transferred form PARTsolutions, then this is always applied (therefrom the density results).
If an exact density has been transferred from PARTsolutions, then the exact density is set[9] without loosing the rest of the physical properties given by the material.
If no exact density has been transferred from PARTsolutions, but an exact mass, then the density is calculated (the volume is given by the model itself | Density = Mass / Volume).
If no material, no mass and no density is transferred from PARTsolutions, then the density cannot be applied.
Direct setting of the volume is not possible, because the volume is defined by the geometric model.
Furthermore direct setting of the mass is not possible. The mass is indirectly set via density by calculation (Density = Mass / Volume).
If both the exact mass and the exact density is transferred from PARTsolutions, then the exact density is set.
[9] That means: if an exact density has been explicitly transferred from PARTsolutions, then this will be used and not the density assigned by the material.