powered by CADENAS

Manual

Manual

5.4.9. Measurement of 3D parts

The Measure dialog is subdivided into fields Element 1, Element 2 and Result and Constraints.

By calling the Measure command the mouse pointer gets a object related geometry symbol in the 3D view , which is signalizing the type of the touched element.

After you have clicked consecutively on two drawing elements(area, edge or bore etc.) in the 3D view a Symbol is displayed in each of the fields Element 1 and Element 2.

In the following the possible geometry symbols are shown:

Bores and cylinders

Conical faces

Circular edges

Planar planes

Straight edge

Toroidal faces

In the following example, the user has clicked on two neighboring faces (see next figure top right).

2 planar planes selected

2 planar planes selected

Fix: The measurement stays during changing the table rows

Fix: The measurement stays during changing the table rows

The two faces are at a specific distance of 10 mm, as shown symbolically in the Result area. The measure of distance (ABS = 10.000°) is displayed to the right of it.

Constraints

With planar, parallel planes the Fix command is available.

Changing the table row the measurement in the 3D view will persist.

With Delete fix. you can delete the constraint.

Transfer

The Transfer command can be used during the classification procedure of native parts.