powered by CADENAS

Manual

Manual

2.5.1.2.2. Parametric Export

In the following the parametric export is described:

  1. In PARTdataManager, choose the desired table.

  2. In the export list field, click on Transfer to CAD (ArchiCAD (Parametric)).

    -> The view switches to ArchiCAD.

  3. Place the exported part with a click on the desired position.

  4. Select the just placed part in the 2D or 3D window. In the 2D window this can only be performed by framing the object (not by clicking).

  5. Click on the object settings in the horizontal bar above the 2D or 3D view.

  6. Select Embedded Library and open the list field under CUSTOM SETTINGS.

  7. Select the desired instance and confirm with OK.

If you want to choose another instance subsequently:

  1. Select the desired part in the 2D or 3D window. In the 2D window this can only be performed by framing the object (not by clicking).

  2. Perform a double-click on the icon Object Tool in the vertical bar on the left of 2D or 3D view.

    -> The dialog box Object Default Settings is opened.

  3. Select Embedded Library and open the list field under CUSTOM SETTINGS.

  4. Select the desired instance and confirm with OK .