Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
...opens the next lower directory level. With objects (single parts/assemblies) the view is switched to the part view.
If you want to keep the old version during the catalog installation, you can open the old versions in the submenu of Versions or add to the part comparison.
Add all versions to part compare:
-> The project versions are loaded in the Part comparison dialog.
For classified parts you can find the command Go to class in the context menu and the corresponding classes in the submenu (one or more).
By clicking on the class, the respective part is opened in the Classes tab page.
Project details (made at creation or changes) (part or assembly) (storage location, name, author, etc.) can be displayed in the Part information dialog box. |
This menu item contains (maximum) the following subitems:
At the following context menu commands, at first the respective dialog box is opened. Then the search may be conducted. The directory to be searched is already set as filter (see under Search in).
Full-text search (see Section 3.1.6.4.2, “ Full-text search ”)
Variables search (see Section 3.1.6.4.3, “ Variables search ”)
Sketch search (2D) (see Section 3.1.6.4.5, “ Sketch search (2D) ”)
Geometric search (3D) (see Section 3.1.6.4.4, “ Geometric search (3D) ”)
Color search (see Section 3.1.6.4.6, “ Color search ”)
Compare parts: Load as first part; Compare parts: Load as second part; Part compare: Add part
These commands are available at project level and within the search results. Herewith you can load parts into the part comparison.
You can find detailed information on this under Komplexe Suche.
The command is only available in the table.
Especially in own part catalogs, where heterogeneous parts with quite different look are collected in a classification project, sorting of the table by geometrical similarity is helpful.
This command is only available at project level. The view sketches are automatically created. These can be modified in the sketcher and then be used for a sketch search.
See Section 3.1.6.4.5.3.2, “ Create sketches automatically from 3D and modify ”.
This command is only available at project level. The respective part is transferred to the Cloud Navigator as root node and then directly the search method Geometric search (3D) is performed.
The menu item Purchineering has the following subitems:
The calling project or directory is inserted in the respective dialog as search source.
Detailed information is found under Section 3.1.14.1, “ Purchineering ”.
The calling project or directory is inserted in the respective dialog as search source.
Detailed information is found under Section 3.1.14.2, “ Duplicates Report ”.
The calling project or directory is inserted in the respective dialog as search source.
Detailed information is found under Section 3.1.14.3, “ Search for unmachined parts ”.
Conduct an Internet search with price comparison.[120]
You can save frequently needed directories or projects on the tabbed page Favorites via context menu command Add to favorites.
You can find the context menu command Add to favorites on the tabbed pages Catalogs, Symbols, Details, Classes, History, Analyses and at search results.
Select the project or directory, which you want to add to "Favorites".
-> The dialog box Add to favorites opens.
In the dialog box the already existing directory structure is displayed.
Now you have the following options:
In the index tree, select the desired directory or, if needed, create further directories via button.
In the list field, under History, select the desired storage path.
At each saving the path is saved as well and added to the history.[121]
-> Now your selection is available on the tabbed page Favorites.
Export favorites / Import favorites
In the Favorites tab you can find the commands Export favorites and Import favorites. Thus you can simply transfer your personal favorites onto another computer. |
|
In PARTdataManager, Part selection, you can find the Analyses tab providing the function Document scan.
Herewith you can perform two things:
Check up-to-dateness of PARTsolutions parts of an assembly loaded in the CAD
Analysis, which parts of an assembly are own parts and which are PARTsolutions parts
Apply Purchineering analysis functions to the result structure (plus manually added further parts as an option)
Via Add to analysis... additional directories and projects can be involved in the analysis.
Detailed information on this can be found under Section 3.1.13, “ Document scan / Analyses ”.
Copy: ...copies the marked object.
|
|
...deletes the selected project/directory from the directory tree.
Note | |
---|---|
Via PARTadmin (see Section 1.3.4.3, “ Icons and display in the index tree” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual) you can include the directory/project again in the structure. |
In order to set up a folder or a whole directory structure below the marked directory, select Create new directory from the context menu. -> The New folder dialog box opens.
|
|
Document projects can be used to append supplementing information (e.g. dimensioning sheets) to a project. Common file formats for this purpose are *.html, *.pdf and *.doc.
The following entries are necessary:
Preview : Storage location of the preview symbol
Open with : If the file format is not known in the system, you can define a program to be started for the document display.
|
Note | |
---|---|
Do not forget %1 at the end of the path declaration! (Placeholder for the file) At English-language operation systems you must use quotation marks in addition ("%1"). |
Preview: Storage location of the preview image
Open with: If the file format is not known in the system, then you can specify a program to be started in order to display the document.
Note | |
---|---|
You can also set the Document types in PARTadmin. On this please see under Section 1.3.7, “ Document types ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |